This is the login for Trane® Connect™ and other Trane® commercial applications. Trane® Connect™ is our secure, cloud-based customer portal to access your building systems to remotely monitor and manage building systems, and conduct routine maintenance.
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
      • AI Building Management
      • Nuvolo Facility Maintenance
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
      • Domestic Hot Water Heat Pumps
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
      • Fan Coil Wall for Data Centers
      • Computer Room Air Handler (CRAH)
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
      • TRACE™
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
      • Trane CDS | Software, Downloads, and Support
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
  • ARIA AI User Interface on Tablet
    AI Building Management
  • Nuvolo Facility Maintenance
    Nuvolo Facility Maintenance
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
  • Domestic Hot Water Heat Pumps
    Domestic Hot Water Heat Pumps
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
  • Fan Coil Wall for Data Centers
    Fan Coil Wall for Data Centers
  • Computer Room Air Handler (CRAH)
    Computer Room Air Handler (CRAH)
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
  • Trane TRACE™
    TRACE™
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
    Trane CDS | Software, Downloads, and Support
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
Commercial Real Estate Data Centers Food & Beverage Federal Government Fulfillment Centers Grocery & Supermarkets Healthcare Higher Education High Tech
Hospitality Indoor Agriculture Industrial K-12 Life Sciences Local Government Restaurants Retail Buildings National Accounts
About Us Contact Us Locate a Sales Office Glossary
Trane Newsroom Customer Stories Trane Blog Events & Webinars Press Releases
CONTACT A TRANE EXPERT
Find Your Trane Rep
Baylor Scott & White Medical Center_960x360.jpg

Customer Story

Baylor Scott & White

Established in 1897, Scott & White Healthcare, now a part of Baylor Scott & White Health, is a leading health care system, encompassing one of the nation's largest multi-specialty group practices that provides personalized, comprehensive health care enhanced by medical education and research. Located on a 98-acre campus, the system’s 119-bed hospital in College Station, Texas, specializes in treating patients experiencing chest pain and heart attacks.

Location: Temple, Texas

Industry: Healthcare

Products Used: Chillers, Air Handling, Controls

Services Used: Upgrading

Climate: Humid & Hot

Topic: Innovation, Efficiency, Cost-Saving, Optimal Comfort, Air Quality, Energy Services

Challenge

As Baylor Scott & White began planning its new medical center in College Station, energy efficiency, doctor retention, patient comfort and safety were priorities. The health care system sought an alternative to boiler heating, common in medical facilities, in order to combat high natural gas and tower makeup water prices. For their operating rooms, Baylor Scott & White was looking for an energy efficient means to achieve the surgeon’s need for cooler and drier air, which often leads to improved patient outcomes and still satisfies temperature and humidity health code requirements. The hospital also wanted to incorporate new technologies to control the circulation of contaminants to reduce airborne disease transmission.

Solution

Based on successful working relationships that spanned many years, Baylor Scott & White assembled its project team for the new facility, relying on the expertise of Jacobs Engineering—and the creative strategic insights of Trane—to design a truly high performance hospital. While hospitals typically use 180 degree hot water from boilers for comfort heating, Trane presented a unique HVAC system design that would use 115 degree water from Trane heat recovery chillers in the upstream position of a series chiller configuration. Although skeptical at first, the hospital and Jacobs Engineering soon became convinced of the significant efficiency benefits achievable with the design paradigm shift.

Improving efficiency with heat recovery

The unique system uses four Trane® CenTraVac™ heat recovery chillers to preheat outside air and for reheat variable-air-volume (VAV) boxes. The heat recovery chillers make 115°F water with NG (natural gas) boilers in a side stream to trim the leaving heat recovery temperature when necessary. While the facility’s heating load is 4.7 MMBH, the chillers can reject up to 11.4 MMBH. Relying on the system to salvage waste heat that would have been discarded to the cooling tower allows the boilers to be turned off 80 percent of the time. Using the boilers only for sterilization and laundry that requires hotter temperatures significantly reduces natural gas consumption.

Controlling critical humidity levels

To control humidity levels in the surgical suites, Trane® Performance Climate Changer™ air handlers with Cool Dry Quiet (CDQ™) desiccant dehumidification wheels were installed. The CDQ desiccant wheel adsorbs water vapor from the process air downstream of the cooling coil, enabling the system to deliver drier supply air at a dew point that is 5°F to 10°F lower than traditional systems. When the wheel rotates, it releases the adsorbed water vapor to the air upstream of the coil, which removes the transferred water vapor via condensation. These air units allow the operating rooms to be cooler and drier as preferred by surgeons.

Reducing transmission of airborne disease

The air handling units include the Trane Catalytic Air Cleaning System (TCACS) air purification. TCACS combines three technologies—MERV 13 high-efficiency filtration, UV-C lights and photo-catalytic oxidation (PCO)—to help control a broad range of biological and chemical airborne contaminants and provide comprehensive air cleaning. A titanium dioxide (TiO2) mesh catalyst is irradiated by UV-C lights, which creates hydroxyl radicals that reduce organic compounds (viruses, mold, bacteria, VOCs) passing through the air handler.

Simplifying facility management

Facility managers use a Trane Tracer™ ES to obtain an enterprise-wide view of the medical complex. The web-based system provides system access via a PC or mobile device to perform daily operations and measure, monitor, analyze and report on environmental conditions.

Results

Embracing a paradigm shift, Baylor Scott & White, Jacobs Engineering and Trane implemented a unique, energy efficient mechanical design for the medical center in College Station, TX. Using 115 degree water from Trane heat recovery chillers in the upstream position of a series chiller configuration, rather than 180 degree hot water from boilers, for comfort heating has reduced natural gas usage by 80 percent, and lowered electrical and water consumption by the cooling towers. Trane Performance Climate Changer air handling units with CDQ and TCAC technologies help to provide a healthy, cool and dry environment in the operating rooms to help meet doctor expectations, enhance the patient experience and reduce infection rates. Pleased with the facility's efficiency and indoor air quality, Baylor Scott & White is making the unique design the standard for its new facilities.

  • Trane ACS Ascend Model Air-Cooled Chiller
    What Is a Chiller?

    Learn what a chiller is, how one works, and the different types you can choose from for your building—all from the experts at Trane Commercial HVAC.

  • tc-connected_buildings-bas-campuses-medium.jpg
    Building Automation System

    Discover what a building automation system is and how it can benefit your organization. Let the experts at Trane help you get the most out of your BAS.

  • Heat Pumps Group
    Electric Heat Pump

    Learn what an electric heat pump is, how it works to cool and heat a building, and its advantages from the experts at Trane Commercial HVAC.