Glossary
Chiller
Learn what a chiller is, how one works, and the different types you can choose from for your building.
Selecting a language changes the language and content on the Trane site.
ComfortSite Login
Trane ComfortSite is an extranet site designed to save you time. With your secure login, you can:
Trane Cloud
Trane Connect is now Trane Cloud—your secure, digital foundation for remotely monitoring and managing building systems, while bringing together insights, applications, and future innovations in one unified experience.
Latin America
Europe
Asia Pacific
Glossary
Learn what a chiller is, how one works, and the different types you can choose from for your building.
In HVAC, a chiller is a critical component of commercial systems designed to cool large buildings by lowering the temperature of a liquid, typically water. The liquid is then circulated throughout the building through a piping system to air handling units (AHUs) that cool the air. Chillers are essential for maintaining comfortable environments in various commercial and industrial settings, including hotels, hospitals, schools, data centers, and manufacturing plants.
Chillers operate on the principle of vapor compression or vapor absorption. Here's how the typical vapor compression chiller works:
The three types of compressors used in Trane chillers are centrifugal, helical rotary, and scroll. Each compressor type offers distinct advantages in terms of efficiency, capacity, maintenance requirements, and cost-effectiveness, depending on the facility's specific cooling needs.
There are two main types of chillers—air-cooled and water-cooled—and each has its own process and considerations.
The process: Air-cooled chillers use fans to blow air over the condenser coils, releasing heat into the atmosphere.
Considerations when determining specifications for air-cooled chillers:
Commonly used for: Small office buildings, data centers, educational institutions, and factories with lower cooling demands, as well as temporary emergency cooling for rental service fleets. Air-cooled chillers are also suitable for process applications, ice making for thermal energy storage, and low-temperature applications, such as ice rinks.
The process: Water-cooled chillers transfer heat from the refrigerant to water, which is then pumped to a cooling tower to release the heat into the air.
Considerations when determining specifications for water-cooled chillers:
Commonly used for: Large commercial buildings, industrial applications, and facilities with significant cooling needs, such as data centers, hospitals, and large manufacturing facilities.
When selecting a chiller, consider factors such as cooling capacity, energy efficiency, noise levels, maintenance requirements, and budget. Consulting with Trane Commercial HVAC professionals can help determine the most suitable chiller for your organization's specific needs.
Resources & Insights
Golden Properties Achieves 73% Energy Savings with Trane’s Chiller Plant Redesign