This is the login for Trane® Connect™ and other Trane® commercial applications. Trane® Connect™ is our secure, cloud-based customer portal to access your building systems to remotely monitor and manage building systems, and conduct routine maintenance.
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
      • AI Building Management
      • Nuvolo Facility Maintenance
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
      • Domestic Hot Water Heat Pumps
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
      • Fan Coil Wall for Data Centers
      • Computer Room Air Handler (CRAH)
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
      • TRACE™
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
      • Trane CDS | Software, Downloads, and Support
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
  • ARIA AI User Interface on Tablet
    AI Building Management
  • Nuvolo Facility Maintenance
    Nuvolo Facility Maintenance
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
  • Domestic Hot Water Heat Pumps
    Domestic Hot Water Heat Pumps
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
  • Fan Coil Wall for Data Centers
    Fan Coil Wall for Data Centers
  • Computer Room Air Handler (CRAH)
    Computer Room Air Handler (CRAH)
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
  • Trane TRACE™
    TRACE™
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
    Trane CDS | Software, Downloads, and Support
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
Commercial Real Estate Data Centers Food & Beverage Federal Government Fulfillment Centers Grocery & Supermarkets Healthcare Higher Education High Tech
Hospitality Indoor Agriculture Industrial K-12 Life Sciences Local Government Restaurants Retail Buildings National Accounts
About Us Contact Us Locate a Sales Office Glossary
Trane Newsroom Customer Stories Trane Blog Events & Webinars Press Releases
CONTACT A TRANE EXPERT
Find Your Trane Rep
tc-exceeding-decarbonization-goals-through-ai-enabled-building-technology.jpg

Customer Story

A Journey to Exceeding Decarbonization Goals through AI-enabled Building Technology

Trane Autonomous Control powered by BrainBox AI® helped an industry leader with decarbonizing its buildings, reducing 1,132 mtCO2e and save $329k in energy costs.

Products Used: Controls, Building Automation Systems

Topic: Sustainability, Decarbonization, AI

An industry leader in the collection and processing of life-saving biological material sought expert guidance on how to advance progress towards Greenhouse Gas (GHG) emission reduction goals. After implementing Trane® Autonomous Control powered by BrainBox AI® in more than 120 donation and collection facilities, Trane Autonomous Control has reduced 1,132 mtCO2e and has resulted in $329k in energy cost savings in the first 18 months of operation.

Motivated by bold sustainability initiatives, a loyal Trane equipment, controls, and services client was seeking expert guidance on how to make progress on aggressive Greenhouse Gas (GHG) reduction goals across a national portfolio of facilities. As an industry leader in the collection and processing of life saving biological material, the client must support both donor comfort and critical product environmental conditions under the same roof.

The decarbonization goals, set by their parent company, included a 40% reduction in GHG emissions by 2025 and to be net zero by 2035.

The Challenge

Due to the critical nature and requirements of the collected biological material, air temperature and humidity control are a matter of life-saving functionality, not just comfort. It was vital to achieve the best possible environmental conditions on a zone-by-zone basis while also helping to optimize energy consumption.

Having already optimized their systems both mechanically and through the use of a Tracer® SC+ Building Automation System, the client needed ways to help generate more significant carbon reduction and cost savings without large investments in human capital or equipment.

Sustainability initiatives needed to fit within their investment threshold and include a crucial stipulation for little to no operational disruptions.

Because no two buildings are identical, it was imperative to create an adaptable program that could be implemented across multiple sites located in different parts of the country.

The Solution

Trane embraced the challenge by introducing a program for decarbonizing buildings that was scalable to the customer’s 150+ donation centers across the country, resulted in significant cost savings, and was implemented with next to no downtime or sizeable equipment investments.

To operate within the customer’s existing parameters, Trane identified an artificial intelligence (AI) enabled solution to predictively optimize the system’s performance.

The unique nature of the client’s business lent itself to the innovative optimization capabilities available through the AI-enabled service, Trane® Autonomous Control powered by BrainBox AI®. By incorporating variables such as predictive weather data, occupancy trends, and equipment performance data, the use of AI technology allows for more advanced optimization to impact the customer's environmental and financial goals.

Without the need for additional hardware, the team avoided impacts from potential supply chain delays, and easily connected from the client’s current building management system to the cloud-based service. It was a seamless coordination between rooftop units and existing internal HVAC equipment which resulted in the transformation of already responsive HVAC systems into predictive systems. This provided the ability to adjust zone-by-zone temperatures autonomously. By monitoring conditions and algorithmically controlling equipment performance, this AI-enabled service helped maximize efficiency and cost savings.

The Results

In the first six months, the client was well over halfway to their 2025 goal at the five test sites—with a 26.1% CO2e reduction and 16.7% savings in electricity. This reduction was accomplished with no additional hardware needed on-site and with no site interruptions.

To date, the program has been implemented at more than 100 additional clinics across the country with impressive results impacting both Scope 1 (natural gas) and Scope 2 (electricity) emissions reductions. The sites that have activated the AI solution have seen a staggering 22% lower Energy Use Intensity (energy / sq. ft.) than sites where Trane Autonomous Control has yet to be activated.

The program proved it could play a large part in reducing the client’s overall carbon footprint and energy costs all while maintaining the strict temperature and humidity requirements necessary for the safety and success of their clinics. These outcomes highlighted the scalability of the program and showed that rapid implementation was possible without disturbance to operations and customer satisfaction.

“The collaborative nature of the development of this program allowed it to be extremely successful,” said Trevor Joelson, a Trane Energy Services Account Executive. “The initial centers showed such great results, the team quickly implemented this in other locations, and the program is delivering significant energy cost savings, making the program cash flow positive.”

As a result of this collaboration, not only did the customer enhance their reputation as a responsible corporate citizen, but they also experienced increased operational efficiency and substantial cost savings. Together, they proved that sustainable practices are not only good for the planet but also beneficial for the bottom line.

Trane® Autonomous Control Powered by BrainBox AI®

Technology that seeks out and implements energy optimization—without human intervention.

Learn More

Trane® Autonomous Control is powered by BrainBox AI®, an AI technology provider that works with collaborators like Trane to empower building owners to reduce their carbon footprint. Trane – by Trane Technologies (NYSE: TT), a global climate innovator – creates comfortable, energy efficient indoor environments through a broad portfolio of heating, ventilating and air conditioning systems and controls, services, parts and supply. For more information, please visit trane.com or tranetechnologies.com.

All trademarks referenced in this document are the trademarks of their respective owners. © 2023 Trane. All Rights Reserved

  • Trane® Ascend™ Air-Cooled Chiller model ACR
    What Is Cooling Capacity?

    Discover what cooling capacity is and how it's used to determine the best size for HVAC systems. The experts at Trane Commercial HVAC explain.

  • Heat Pumps Group
    Electric Heat Pump

    Learn what an electric heat pump is, how it works to cool and heat a building, and its advantages from the experts at Trane Commercial HVAC.

  • Team Meeting of Renewable Energy Engineers Working on an Innovative More Efficient Solar Panel Battery Concept. Group of Specialists Gathered Around Table, Solving Problems. Bright Research Facility
    Can Your Building Operate More Efficiently?

    Understanding your building’s energy use is a vital first step in helping to improve energy efficiency. Knowing who to trust to interpret the data and guide next steps is just as important.