This is the login for Trane® Connect™ and other Trane® commercial applications. Trane® Connect™ is our secure, cloud-based customer portal to access your building systems to remotely monitor and manage building systems, and conduct routine maintenance.
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
      • AI Building Management
      • Nuvolo Facility Maintenance
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
      • Domestic Hot Water Heat Pumps
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
      • Fan Coil Wall for Data Centers
      • Computer Room Air Handler (CRAH)
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
      • TRACE™
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
      • Trane CDS | Software, Downloads, and Support
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
  • ARIA AI User Interface on Tablet
    AI Building Management
  • Nuvolo Facility Maintenance
    Nuvolo Facility Maintenance
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
  • Domestic Hot Water Heat Pumps
    Domestic Hot Water Heat Pumps
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
  • Fan Coil Wall for Data Centers
    Fan Coil Wall for Data Centers
  • Computer Room Air Handler (CRAH)
    Computer Room Air Handler (CRAH)
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
  • Trane TRACE™
    TRACE™
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
    Trane CDS | Software, Downloads, and Support
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
Commercial Real Estate Data Centers Food & Beverage Federal Government Fulfillment Centers Grocery & Supermarkets Healthcare Higher Education High Tech
Hospitality Indoor Agriculture Industrial K-12 Life Sciences Local Government Restaurants Retail Buildings National Accounts
About Us Contact Us Locate a Sales Office Glossary
Trane Newsroom Customer Stories Trane Blog Events & Webinars Press Releases
CONTACT A TRANE EXPERT
Find Your Trane Rep
Penn Highlands Mon Valley Building

Customer Story

Penn Highlands Mon Valley

Penn Highlands Mon Valley (formerly Monongahela Valley Hospital) upgraded its aging chiller plant with Trane's high-efficiency system, reducing energy costs and improving comfort without any downtime.

Location: Monongahela, Pennsylvania

Industry: Healthcare

Products Used: Chillers, Controls

Services Used: Upgrading

Topic: Efficiency

Facility Size: 280,000 sq ft

Summary

Penn Highlands Mon Valley (formerly Monongahela Valley Hospital) is a 280,000 sq ft, 226-bed, full-service health care facility with 1,100 employees, including a 220-member medical staff representing more than forty specialties. In addition to the plethora of services offered, Penn Highlands Mon Valley offers resources and support to the community. The 100-year-old hospital strives to provide the highest quality care to its patients, as well as comfort and convenience to family members and friends.

Challenge

The aging chiller plant at Penn Highlands Mon Valley, installed in the 1970s, was nearing the end of its useful life. With the hospital running 24/7, and the nature of its work, facility managers knew it was critical that the chiller plant be upgraded quickly. The chiller plant upgrade and integration of the control systems would need to be performed while Penn Highlands Mon Valley continued to use the existing equipment, in order to adhere to the hospital’s zero cooling system downtime requirements. In addition to keeping its patients and staff comfortable, the hospital set a goal to lower energy costs.

Solution

Penn Highlands Mon Valley called on the expertise of Trane to provide a complete turnkey solution to meet the challenges of its chiller plant replacement.

Modular design speeds installation

To save installation time, a packaged pre-built modular chiller plant was delivered to the site in three sections and assembled within a new pre-piped and pre-wired enclosure. Designed to fit in the tight space requirements outlined by the hospital, the compact chiller plant was placed on a concrete pad in a small area outside the building. A steel structure was built above the new plant enclosure to hold the two cooling towers.

New chillers improve efficiency, reliability

Two 400-ton high-efficiency Trane CenTraVac™ centrifugal chillers were installed. The robust design of the Trane CenTraVac centrifugal chiller, with only one moving part, makes it one of the most reliable in the industry and the right choice to meet the hospital’s zero cooling system downtime criteria. The CenTraVac chiller requires less refrigerant to operate and its semi-hermetic motor design, along with low-pressure refrigerant, reduces refrigerant leaks, assuring a clean, cool operation for maximum performance. The quiet, vibration-free operation of the chiller also helps the hospital maintain a restful environment for its patients.

VFDs, heat exchangers provide energy savings

The chiller plant includes an energy-saving heat exchanger to allow free cooling in cooler months, and variable frequency drives (VFDs) on the CenTraVac chiller, the chilled water and condenser water pumps, and the cooling tower fans. The VFDs reduce energy usage, extend motor life and help to maximize the comfort of patients and staff.

Control system allows easy monitoring

A Trane Tracer™ SC control system automates the chiller plant and integrates fully through BACnet® with the existing third party vendor’s HVAC controls system already used by the hospital. The web-based controller with graphics provides an easy-to-use interface via the web to monitor and control the chiller plant from any location. The management tool helps improve efficiencies, reduce energy costs and increase comfort. Facility managers use the Tracer SC to optimize energy efficiency with chiller sequencing routines, coordinate the pump and cooling tower to reduce costs, and use diagnostic messages for troubleshooting.

TIS ensures fast issue resolution

A Trane service contract ensures the peak performance of the equipment and reduces service costs with a regular maintenance plan versus emergency service calls. Trane® Intelligent Services (TIS) Active Monitoring provides peace-of-mind to building managers with constant monitoring of systems, alarm notification, diagnostics and analysis by Trane technical specialists. Continually collecting and interpreting data from the building equipment and controls, TIS allows responsive action should an issue arise.

Results

Penn Highlands Mon Valley replaced its aging chiller with a new Trane high efficiency chilled water plant, which includes two Trane 400-ton CenTraVac™ chillers, a free cooling heat exchanger, and VFDs on the chillers, water pumps and cooling tower fans. A new Trane Tracer SC controller was integrated into the existing control system for easy monitoring of the fully-automated chiller plant. The upgrades, which were completed without disruption to hospital operations, are reducing energy and maintenance costs, increasing efficiencies and helping to ensure a comfortable indoor environment for patients and staff.

"The efficiency of the chilled water plant has exceeded our expectations,” said William Burnett, director of engineering and maintenance, Monongahela Valley Hospital. “The second chiller was not even needed during our July heat wave.”

About Penn Highlands Mon Valley 

A packaged pre-built modular chiller plant installed at Penn Highlands Mon Valley includes two 400-ton high-efficiency Trane CenTraVac centrifugal chillers.

A Trane Tracer SC controller was integrated with existing controls without a single moment of downtime.

  • tc-connected_buildings-bas-campuses-medium.jpg
    Building Automation System

    Discover what a building automation system is and how it can benefit your organization. Let the experts at Trane help you get the most out of your BAS.

  • Heat Pumps Group
    Electric Heat Pump

    Learn what an electric heat pump is, how it works to cool and heat a building, and its advantages from the experts at Trane Commercial HVAC.

  • M Series Indoor Unit - MSY
    What Is a Mini-Split HVAC System?

    Discover the potential benefits of a mini-split HVAC system. The experts at Trane explain how they work, their commercial applications and more.