This is the login for Trane® Connect™ and other Trane® commercial applications. Trane® Connect™ is our secure, cloud-based customer portal to access your building systems to remotely monitor and manage building systems, and conduct routine maintenance.
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
      • AI Building Management
      • Nuvolo Facility Maintenance
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
      • Domestic Hot Water Heat Pumps
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
      • Fan Coil Wall for Data Centers
      • Computer Room Air Handler (CRAH)
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
      • TRACE™
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
      • Trane CDS | Software, Downloads, and Support
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
  • ARIA AI User Interface on Tablet
    AI Building Management
  • Nuvolo Facility Maintenance
    Nuvolo Facility Maintenance
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
  • Domestic Hot Water Heat Pumps
    Domestic Hot Water Heat Pumps
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
  • Fan Coil Wall for Data Centers
    Fan Coil Wall for Data Centers
  • Computer Room Air Handler (CRAH)
    Computer Room Air Handler (CRAH)
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
  • Trane TRACE™
    TRACE™
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
    Trane CDS | Software, Downloads, and Support
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
Commercial Real Estate Data Centers Food & Beverage Federal Government Fulfillment Centers Grocery & Supermarkets Healthcare Higher Education High Tech
Hospitality Indoor Agriculture Industrial K-12 Life Sciences Local Government Restaurants Retail Buildings National Accounts
About Us Contact Us Locate a Sales Office Glossary
Trane Newsroom Customer Stories Trane Blog Events & Webinars Press Releases
CONTACT A TRANE EXPERT
Find Your Trane Rep

Customer Stories

High Museum Of Art

CHOOSING THE COMPANY ISN’T JUST ABOUT PRICE; IT’S ABOUT PRICELESSNESS

Short On Time, With No Room For Error, The High Museum Calls On Trane

To Get a Major Show, The High Museum Must Get It Right.

The High Museum had just completed a major expansion that added five buildings and doubled the museum’s size, and in doing so had attracted an exhibition of world masterpieces from legendary museums like France’s Musee du Louvre. But as Marjory Harvey, Director of Architectural Planning and Design, can tell you, attracting world-class shows is not as simple as just having an amazing space. "Proper climate control is essential to a museum’s ability to attract important gifts, loans and exhibitions. We are often required to demonstrate our ability to meet and maintain environmental standards for the preservation of works of art." Certainly Trane was up to that challenge, but the High Museum needed their new system fast-tracked so the museum could provide a record of gallery temperature and humidity conditions to finalize an agreement with the Louvre and bring the show to Atlanta.

A World-Class System Is The Only Thing That Will Do.

The High Museum already had two existing Trane chillers installed in 1982 and they were still running smoothly, so it was decided to supplement them with a new chiller plant. The new chillers include a Trane 450-ton heat recovery centrifugal chiller (for winter heating needs) and a 500-ton high efficiency chiller. The pièce de résistance however, was Trane’s sophisticated Climate Changer™ air handlers, and 101 VAV units all orchestrated by a Tracer Summit building automation system.

The High Museum Gets High Marks.

Trane’s Tracer Summit™ system allows the museum precision control of their climate. It maintains temperature and humidity at 72 degrees Farenheit, plus or minus 2 degrees, and 50 percent humidity, plus or minus five percent. This degree of control assures that priceless paint and other materials do not become too dry and chip, or too damp, as excess humidity can cause mold, fading, chemical reactions and myriad other disasters. Since installing their new Trane system the High Museum’s collection has nearly doubled in size and membership is among the top 10 in the U.S. And Trane is happy to report, the museum got the Louvre show—for a three-year engagement.

 

About High Museum Of Art

High Museum attendance is nearly 450,000 visitors a year, the collection has nearly doubled and membership is among the top 10 of any art museum in the U.S. The museum played a key role in transforming Midtown into one of Atlanta’s most robust areas. During the next three years, "Louvre Atlanta" at The High will highlight the history of the Louvre from the 17th Century to present. Three exhibitions during the first year will focus on the establishment of the royal art collection in "Kings As Collectors" and feature works by Raphael, Rembrandt, Vaelazquez, Murillo and Poussin, and a group of sculptures that interpret King Louis XIV’s role as collector and arts patron.

High Museum of Art hero.JPG