This is the login for Trane® Connect™ and other Trane® commercial applications. Trane® Connect™ is our secure, cloud-based customer portal to access your building systems to remotely monitor and manage building systems, and conduct routine maintenance.
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
      • AI Building Management
      • Nuvolo Facility Maintenance
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
      • Domestic Hot Water Heat Pumps
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
      • Fan Coil Wall for Data Centers
      • Computer Room Air Handler (CRAH)
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
      • TRACE™
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
      • Trane CDS | Software, Downloads, and Support
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
  • ARIA AI User Interface on Tablet
    AI Building Management
  • Nuvolo Facility Maintenance
    Nuvolo Facility Maintenance
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
  • Domestic Hot Water Heat Pumps
    Domestic Hot Water Heat Pumps
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
  • Fan Coil Wall for Data Centers
    Fan Coil Wall for Data Centers
  • Computer Room Air Handler (CRAH)
    Computer Room Air Handler (CRAH)
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
  • Trane TRACE™
    TRACE™
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
    Trane CDS | Software, Downloads, and Support
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
Commercial Real Estate Data Centers Food & Beverage Federal Government Fulfillment Centers Grocery & Supermarkets Healthcare Higher Education High Tech
Hospitality Indoor Agriculture Industrial K-12 Life Sciences Local Government Restaurants Retail Buildings National Accounts
About Us Contact Us Locate a Sales Office Glossary
Trane Newsroom Customer Stories Trane Blog Events & Webinars Press Releases
CONTACT A TRANE EXPERT
Find Your Trane Rep

Cold Ahead: Prepare Your Facility Now

November 11, 2020

modern business hall interior with glass wall

With 2020 driving unprecedented demands – at work and home – you may not yet have prepared your building for colder days.

There’s still time! Here are a few tips and recommendations from Trane® building professionals that can help you save energy and lower your utility bills during the colder months ahead.

1. Understand building changes

The way your building is used — and the hours it is occupied — may change anytime winter arrives but especially this year, depending upon whether tenants are working from home or heading into the office. Review building and system data to monitor occupancy rates and adjust equipment and system setpoints to support the current usage needs. Use automatic scheduling to reduce the building’s energy consumption during the holidays, when your building will likely be unoccupied.

2. Avoid problems with proper maintenance

Proper maintenance is critical — an equipment outage is the last thing you want in the middle of a snowstorm or if your state requires additional lockdowns. Check HVAC systems and equipment to determine if they are working correctly. Change filters and look for cracks in the heat exchanger to optimize system performance. You should also check the boiler and stroking valves to confirm the outside air intakes are on the lowest setting.

3. Use your economizer wisely

In many parts of the country, colder months bring dry weather with low humidity, which is perfect for taking advantage of an economizer. An air-side economizer uses the cooler outside air to reduce the indoor temperature, which is more energy efficient than cooling the recirculated indoor air. Many buildings have break-even points — the temperature at which the building starts using mechanical cooling — of 60 degrees Fahrenheit or less. In many cases, the building can be pre-cooled with outside air to run a little cooler in the mornings, so the occupied setpoint can slowly rise during the day — without compromising occupant comfort.

4. Conduct a building walk-through

One easy way to spot energy savings and improve efficiency is to conduct a walk-through. A visual inspection can help you uncover deficiencies that are often easily fixed. For example, keep an eye out for space heaters being used in certain parts of your building. Consider the reasons why these zones are running cooler than others and how this can be addressed.

Check the building envelope during your inspection process. Verify that all exterior doors and windows are closing and sealing properly, and roof drains and filters are clear from debris.

5. Review your plans

Equipment breakdowns and weather-related outages can happen any time of year, so it’s important to have a contingency plan in place that addresses your needs in colder months. Your contingency plan should outline the processes and steps you will take to keep your building running in the event of an outage or emergency. This year, it also should address how you will keep it running should an unexpected lockdown occur in your area.

6. Know your utility rates

Utility demand charges are typically more severe in the summer months, but you still have opportunities to reduce or shift demand during the colder months to help lower costs.

Knowing your utility billing dates is important as the seasons change. For example, if your billing cycle ends on Dec. 15, and Dec. 16 and 17 prove to be unseasonably warm days, try to find ways to cool your building other than running the chiller for that brief window — which can cause an expensive spike in demand charges for the entire month.

Don’t let winter sneak up on you. Now is the time to make sure your building is prepared for the colder temperatures, and Trane is your partner in this effort. Trane building professionals are ready to help you determine your winter readiness and provide additional recommendations for improvement.