This is the login for Trane® Connect™ and other Trane® commercial applications. Trane® Connect™ is our secure, cloud-based customer portal to access your building systems to remotely monitor and manage building systems, and conduct routine maintenance.
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
      • AI Building Management
      • Nuvolo Facility Maintenance
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
      • Domestic Hot Water Heat Pumps
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
      • Fan Coil Wall for Data Centers
      • Computer Room Air Handler (CRAH)
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
      • TRACE™
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
      • Trane CDS | Software, Downloads, and Support
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
  • ARIA AI User Interface on Tablet
    AI Building Management
  • Nuvolo Facility Maintenance
    Nuvolo Facility Maintenance
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
  • Domestic Hot Water Heat Pumps
    Domestic Hot Water Heat Pumps
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
  • Fan Coil Wall for Data Centers
    Fan Coil Wall for Data Centers
  • Computer Room Air Handler (CRAH)
    Computer Room Air Handler (CRAH)
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
  • Trane TRACE™
    TRACE™
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
    Trane CDS | Software, Downloads, and Support
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
Commercial Real Estate Data Centers Food & Beverage Federal Government Fulfillment Centers Grocery & Supermarkets Healthcare Higher Education High Tech
Hospitality Indoor Agriculture Industrial K-12 Life Sciences Local Government Restaurants Retail Buildings National Accounts
About Us Contact Us Locate a Sales Office Glossary
Trane Newsroom Customer Stories Trane Blog Events & Webinars Press Releases
CONTACT A TRANE EXPERT
Find Your Trane Rep
  1. Trane Commercial HVAC
  2. About Us
  3. Newsroom
  4. Trane Commercial Blog
  5. Open systems in building management systems

Open systems in building management systems

By: Chuck Lehn, Open Systems Application Engineer, Trane

November 03, 2021

  

When it comes to building management systems (BMS), not everyone defines “open systems” the same. When people talk about open systems, their discussion falls into three categories: open distribution, open protocols and open service.

In this blog, we will explore open protocols.

Open, Standard Protocols
A communication protocol is a set of rules used to share data. An open protocol means the communication rules are publicly available. Using an open protocol is a good first step but can become complicated if a single vendor owns the protocol. That vendor could keep some of the features for only their products, making it less open than would first appear. Or worse, the vendor may change the protocol leaving existing systems in a state where an upgrade may break existing interoperability.

An open, standard protocol is not only publicly available but was created and is maintained by an industry group. This industry group should be comprised of manufacturers, system integrators, and end users so everyone’s needs are considered.

In the BMS market, BACnet is the most commonly used open, standard protocol.  

Why should I care about open, standard protocols?
Open, standards may be one of the most boring aspects of our industry (not to me though ) but they are critical to create an open system.

  • Product Certification: An open, standard protocol will have an independent group perform product certification to ensure products adhere to the standard. This ensures a higher probability of interoperability.
  • Troubleshooting Tools: Product certification helps minimize integration issues but doesn’t eliminate all issues. Open standards enable multiple vendors to create troubleshooting tools to help with integration issues, rather than having no option other than  a vendor specific tool.
  • Protocol Enhancements: An active standards group is a great sign the protocol is doing well in the industry and can adapt to add functionality that may not have been considered in the past. Since the standards groups have representation from different sources, these enhancements are widely shared  and are backward compatible. For example, as cyber security has become more important in recent years, ASHRAE® SSPC 135 (BACnet) has added BACnet Secure Connect (BACnet/SC) as a new secure, encrypted data link to adapt to the industry need.  

Application Programming Interface (API)
There has been a lot of discussion (and confusion) about using APIs for BMS integration. What is an API?

An Application Programming Interface (API) allows two software applications to share data. The first application sends a request to the other application and the second application returns a response. The API defines these requests and responses.

A protocol is the set of rules describing how the requests and responses get to the applications.

In the BMS world, BACnet is an open, standard protocol that defines both these concepts. However, many other systems will provide an API for integration.

Why use an API?
The BMS industry has been using BACnet for many years. Other industries have never heard of BACnet and prefer to use other protocols or APIs that better meet their needs. An API is a faster and easier way to share data for a software developer rather than developing an open, standard protocol. Typically, one vendor creates the API to suit their needs and provides the API documentation to the other vendor. The second vendor then needs to develop their application to use the API. This means each API is custom development for the other vendor. This is very similar to an open protocol (not an open standard protocol) in that the vendor that owns the API can keep some of the API functionality exclusive  or make updates to the API that can impact  existing installations.

APIs need to be well understood before implemented in a BMS. APIs are a quick way to provide a mechanism to integrate, but they come with a larger amount of upfront labor and need to be maintained, both of which represent costs to a solution. Some considerations when considering an API would be:

  • What happens when communication is lost between the two systems?
  • How do you troubleshoot the API or get support for the API?
  • How will we maintain functionality when the API is changed to a new version?

Meeting Customer Needs
The goal of open systems is to meet customer needs. One of the most effective parts of an open system are open, standard protocols. Why?

  1. Flexibility to choose products: Choose the best-in-class products that can integrate to multiple vendors by specifying BACnet Testing Laboratories (BTL) listed BACnet products.
  2. Open data collection: Choose open, standard protocols so all data is available to multiple vendors at any level of the architecture.
  3. Open, flexible infrastructure: Choose open, standard protocols to ensure interoperability now and in the future.
  4. Open service, open tools: Choose open, standard protocols so multiple vendors can service the BMS and tools are readily available.

About the Author

Chuck Lehn

Chuck Lehn, Systems Application Engineer

Chuck Lehn is a Trane systems application engineer based out of St. Paul, Minnesota. He offers more than 20 years of controls products experience working with many Trane and non-Trane solutions in a diverse range of vertical markets. Chuck is primarily responsible for system integration, product development, and sourced controls products. He supports the presales and technical support teams and is the lead instructor for the Trane University - System Integration class.

Chuck graduated from South Dakota State University with a Bachelor of Science degree in mechanical engineering. Chuck and his family reside in Minnesota.

  

Read More About Open System Building Controls

  • Chuck Lehn.jpg

    Open systems in building management systems

    A communication protocol is a set of rules used to share data. An open protocol means the communication rules are publicly available. Using an open protocol is a good first step but can become complicated if a single vendor owns the protocol. That vendor could keep some of the features for only their products, making it less open than would first appear. Or worse, the vendor may change the protocol leaving existing systems in a state where an upgrade may break existing interoperability.
  • open systems 5 tips

    Open distribution in building automation systems

    When it comes to building automation systems, not all uses of the term “open system” are equal. When talking about open systems, definitions typically fall into three categories: open distribution, open protocols, and open service. This blog explores open distribution.
  • Chuck Lehn.jpg

    Five Tips to Navigating the Complexity of Open System Building Controls

    When it comes to building automation systems, not all uses of the term “open system” are equal. The following tips can help you identify the most critical open system capabilities so you can make an informed decision for your building or project’s needs.