CONTACT A TRANE EXPERT

On-site Training

Airside System Service

  • 4.5 days
  • 3.2 CEU's

This course covers the operation and setup of a commercial VAV system from the standpoint of the service technician. Shutoff VAV, Bypass VAV and Single Zone VAV will be discussed in the class, although Shutoff VAV (traditional VAV) will be the primary focus. The concepts discussed will apply to new system startup as well as existing buildings. The course also discusses the different fan types used in commercial HVAC units. The course includes systems used in all geographic regions.



The lab exercises are designed around several working VAV systems in our La Crosse, Wisconsin, training lab. This includes IntelliPak® Commercial Self-Contained (CSC) and rooftop units (RTU) with various types of VariTrane® VAV boxes. During the lab exercises, students will use the various tools and software needed to setup and commission (or re-commission) a VAV system. Attendees will learn to recognize important parameters within building plans in order to commission the building as the design engineer intended. The plans used will include the equipment schedule, sequence of operation, airflow requirements, and ventilation.


Upon completion of this course, participants should be able to
  • Verify system airflow using multiple methods.
  • Interpret fan curve data from the various fan types such as forward curve, airfoil, and direct drive plenum.
  • Set up and verify proper system air with the fan types used in our lab.
  • Describe the capabilities and the limitations of the building control system from a service technician standpoint.
  • Using a Rover service tool, analyze air delivery on multiple VAV systems.
  • Describe the difference between Single Zone VAV systems and Multiple Zone VAV systems.
  • Go through the procedure required to establish the supply pressure setpoint on a VAV system.


Our programs use a variety of assessment methods to measure learning, from pre and post tests, to classroom activities, quizzes and workshops.


Next Class

2213 20th Street S, Bldg 12, La Crosse, WI, 54601

Nov 16-20, 2020

$1800

9 seats available

An early bird discount of 10% off tuition will be given when you register more than 60 days prior to the start date. We also have Package Programs where you can save up to 40% off tuition of multiple courses! Visit our website for more details www.trane.com/traneuniversity

Locations & Dates

2213 20th Street S, Bldg 12, La Crosse, WI, 54601 Nov 16-20, 2020 $1800 9 seats available Register