Trane Introduces New XStream™ RTHF G

Brussels, Aug. 14, 2018 – Trane®, a leading global provider of indoor comfort solutions and services, and a brand of Ingersoll Rand, introduces RTHF G, the newest addition in the XStream™ range of water-cooled screw chillers. The new design, now available in countries across Europe, Middle East and Africa, is part of the Ingersoll Rand EcoWise™ portfolio, designed to lower environmental impact with next-generation, low-global warming potential (GWP) refrigerants and high-efficiency operation.

“RTHF G units address the needs of building owners who want to increase the sustainability of their operations, while maintaining or improving capacity, efficiency and reliability with critical, large capacity cooling installations,” said Jose La Loggia, vice president and general manager of Trane in Europe. “We’re proud to continue offering customers new options for sustainability without sacrificing quality, reliability or performance. Our innovations are consistent with the Ingersoll Rand global Climate Commitment, which includes providing customers with products that help reduce the greenhouse gas footprint of refrigerants and provide lower global warming potential alternatives.”

The new design offers customers an alternative, cost-effective option for reducing greenhouse gas emissions, because the units operate with R-1234ze, a near zero GWP refrigerant. This makes Trane RTHF G units unique on the market today as the only chillers in this capacity range to operate with a near-zero GWP refrigerant, and deliver high seasonal efficiency, low installation footprint and stable part load control at all conditions.

The new units feature the largest screw compressors on the market, which when used in a double circuit deliver capacity of up to 2700 kilowatts (kW) and benefit most commercial and industrial cooling applications that require maximum performance and sustainability within a limited installation space. The design of the XStream RTHF G offers reliable, high-efficiency performance with up to 6.3 Energy Efficiency Ratio (EER) and up to 9.5 European Seasonal Energy Efficiency Ratio (ESEER) with variable speed.

The key differentiators of the new XStream RTHF G screw chillers include:

-Dual circuit configuration in a market segment that could previously only use single circuit centrifugal chillers. Dual circuit configuration reduces refrigerant content per circuit and further increases reliability

-Serial counterflow design compatible with the use of variable primary flow used for the first time in a screw compressor chiller and allowing for a greater efficiency.

For more details of on the complete Trane portfolio of solutions, please visit Trane.com.

About the Ingersoll Rand Climate Commitment

In 2014, Ingersoll Rand publicly committed to increase its energy efficiency and reduce the greenhouse gas emissions (GHG) related to its operations and products. The company’s Climate Commitment includes:

·         50 percent reduction in GHG refrigerant footprint of its products by 2020 and lower-GWP alternatives across its portfolio by 2030;

·         $500 million investment in product-related research and development to fund long-term GHG reduction

·         35 percent reduction in the greenhouse gas footprint of its own operations by 2020

Ingersoll Rand’s Climate Commitment has enabled the avoidance of 11 million metric tons of CO2e globally from its products compared to a 2013 baseline, equal to the emissions from the energy used in 1.6 million homes for one year. The company also has reduced the GHG intensity of its operations by 23 percent when compared to a 2013 baseline.

 

# # #

About Ingersoll Rand

Ingersoll Rand (NYSE:IR) is a world leader in creating and sustaining safe, comfortable and efficient environments in commercial, residential and industrial markets. Our people and our family of brands — including Club Car®, Ingersoll Rand®, Thermo King® and Trane® — work together to enhance the quality and comfort of air in homes and buildings, transport and protect food and perishables, secure homes and commercial properties, and increase industrial productivity and efficiency. Trane solutions optimize indoor environments with a broad portfolio of energy efficient heating, ventilating and air conditioning systems, building and contracting services, parts support and advanced control. Ingersoll Rand is a $14 billion global business committed to sustainable business practices within our company and for our customers. For more information, visit www.ingersollrand.com or www.trane.com.

Contact Information

Heidi McGuire

651-407-4000

heidi.mcguire@irco.com