Data Center Cooling & Thermal Management for AI Workloads, Hyperscale & Colocation Facilities

Trane delivers end-to-end thermal management for hyperscale and colocation data centers, solving the toughest challenges in AI workload cooling and energy optimization.

Overview

How can Trane help unlock the potential in your thermal management strategy?

AI workloads are raising density, changing load profiles and pushing data center cooling systems to do more. Stronger performance starts before equipment is selected, when the full thermal management strategy is designed around the way the site needs to operate.

That’s why Trane starts with collaboration. We work alongside your team to understand your goals, your site’s thermal requirements, your sustainability targets and where you need room to grow. Then our data center engineering specialists use modeling, validation and reference designs to help turn those goals into clearer cooling decisions.

From there, Trane helps connect cooling equipment, controls, data and service expertise across the chiller plant and data hall. This systems-based approach supports uptime while helping your team plan for capacity, efficiency, water strategy and future scale.


Data center performance rules have changed; the future is now.

Our Approach

How does Trane deliver collaborative data center cooling solutions?

The process starts with your site, your goals and the way your facility needs to operate. Trane works with your team early to understand site requirements, operating needs, sustainability targets and growth plans. From new builds to retrofits, our specialists help shape a thermal management strategy before design choices become harder to change.

Data centers are being built for tenants who may not know today what their cooling needs will look like five years from now. A room planned for one level of power density could end up supporting far more heat as equipment changes, which can create real headaches if the infrastructure was only sized for opening day. The goal is not just to have enough capacity on Day 1, but to build a cooling system that can grow with the facility over time—without replacing chillers, tearing back into the building, or re-running conduit just to keep up.

  • This is where the work starts to come into focus. Trane brings your team and our experts together to define goals, review operating needs and set the parameters that guide the cooling strategy.

    Two Businesswomen Working On Computer In Office

Reference Designs

How do Trane’s data center reference designs help accelerate scalable, AI-ready infrastructure?

Once the strategy begins to take shape, Trane reference designs help teams move from early planning to clearer cooling decisions. Use them to compare system strategies, evaluate air and liquid cooling approaches, and plan for redundancy, energy use, water strategy and growth.

Each design gives engineers a practical starting point they can adapt to the site, load profile, and long-term operating goals.


Conceptual image of data center heat resulting from AI workloads

Products & Solutions

How do Trane chillers, CDUs, and controls act as an integrated data center cooling system?

With the strategy and system design defined, Trane helps bring your thermal management ecosystem together. Cooling equipment, controls and services are coordinated across the cooling path to help data center teams plan, operate and adapt thermal infrastructure as AI workloads and density grow.


Sustainability and Performance

How can Trane's custom thermal management solutions enhance data center energy efficiency?

When cooling strategy, equipment, controls and service are planned as one system, sustainability decisions can be built in earlier. We help your team evaluate choices such as free cooling, heat recovery, water use and long-term service so you can manage higher loads while balancing energy use, water strategy and emissions.

Higher data center densities are opening new opportunities for liquid cooling, heat reuse, energy efficiency, and more sustainable growth.

Insights

Data Center Case Studies, Whitepapers & Insights

  • Data Center Green Sustainability
    • Blog

    How Temporary Thermal Management Supports the Data Center Lifecycle

    Discover how temporary thermal management can support data center construction, commissioning, load testing, maintenance and uptime throughout the facility lifecycle.

    October 02, 2026

  • Shot of Data Center With Multiple Rows of Fully Operational Server Racks. Modern Telecommunications,Data center cooling,server room,3d rendering
    • Blog

    What Is a Data Center?

    Learn what a data center is, the different types, and how data center sustainability can be a reality with the proper design and optimization.

    September 17, 2026

  • Data Flow: A frozen cascade of water symbolizes the flow of data in a modern server room, highlighting the essential role of water in cooling and maintaining these powerful systems.
    • Blog

    Smart Water Strategy: Better Data Center Cooling

    Smarter thermal management helps data centers balance water use, energy efficiency, resilience and future AI growth by aligning cooling strategy with workload, site risk and sustainability goals.

    August 31, 2026

  • A engineer under checking the industry cooling tower air conditioner is water cooling tower air chiller HVAC of large industrial building to control air system.
    • Blog

    Data Center Cooling Reliability: Reduce Outages

    Learn how reliable data center cooling helps reduce outages through redundancy, monitoring, airflow management and preventive maintenance that support uptime and resilience.

    August 11, 2026


  • Data Center AI Factory
    • Event

    DCD>Connect | Virginia

    Join Trane at DCD Connect Virginia, November 3–4 at Lansdowne Resort in Leesburg, Va., to explore resilient, efficient data center cooling strategies.

    October 01, 2026

  • Servers data center room with bright bokeh light going through the corridor 3D rendering
    • Event

    Yotta Las Vegas 2026

    From concept to deployment, discover how Trane’s deep collaboration helps enable speed and scale for AI factory infrastructure.

    September 25, 2026

  • data center
    • Whitepaper

    Building Trust at Scale: Strategies for Data Center Sustainability

    A practical look at how data centers can scale sustainably through efficient thermal design, lower water use, reduced emissions, and stronger community trust.

    August 06, 2026

  • White storage and processing unit, large AI processing server room, data center storage and network processing room, SSD and hard disk drive storage, and processor cooling system,3D rendering

    Rethinking Water Usage in Data Centers

    Water consumption is a critical design factor for larger data center designs seeking a balance between power and water usage.

    April 30, 2026

Events

Data Center Trade Shows, Webinars & More


FAQs

Your top data center questions, answered.

Trane provides tailored data center cooling solutions, ensuring optimal performance, energy efficiency, and reliability. Our offerings include advanced cooling technologies like precision cooling, liquid cooling, and free cooling to reduce energy consumption. We offer modular cooling solutions for scalable capacity and data center HVAC systems that optimize airflow and heat dissipation with features like hot and cold aisle containment. Our energy-efficient HVAC units have advanced controls for real-time adjustments. Trane also provides energy management services with DCIM tools for real-time insights into energy use, temperature, and airflow. We integrate renewable energy sources and offer energy-efficient hardware aligned with sustainability initiatives. Our experts collaborate with clients to develop customized solutions from design to support, helping data centers achieve energy savings, enhanced performance, and reliable operations.

Reducing energy consumption and improving data center energy efficiency can be achieved through several strategies. Optimize cooling systems with advanced techniques such as liquid cooling or immersion cooling and regular maintenance. Improve server utilization by consolidating workloads, using virtualization, and implementing dynamic power management. Choose facility level systems that utilize free cooling when ambient conditions allow. Upgrade to energy-efficient hardware and opt for SSDs and high Energy Star ratings. Use energy management software to monitor and manage usage and enhance power distribution with efficient PDUs and UPS. Adopt renewable energy sources, purchase renewable energy credits, and partner with green energy providers. Conduct regular audits to identify inefficiencies and continuously monitor energy usage.

A sustainable or green data center minimizes environmental impact and maximizes energy efficiency. These centers use energy-efficient hardware, advanced cooling techniques, and optimized power management, often measured by Power Usage Effectiveness (PUE). They prioritize renewable energy sources like solar, wind, or hydroelectric power and may purchase renewable energy credits (RECs). Efficient cooling systems and resource conservation practices, such as water-efficient cooling and recycling electronic waste, are key. Green data centers aim to reduce their carbon footprint and often seek certifications like LEED or ENERGY STAR. Continuous monitoring and optimization through data center infrastructure management (DCIM) tools help maintain efficiency.

Meeting data center sustainability goals amid rising energy demands requires a multifaceted approach. Optimize energy usage with advanced cooling techniques like liquid cooling and free cooling, and hot/cold aisle containment. Invest in energy-efficient hardware with high Energy Star ratings. Use virtualization to maximize server utilization and reduce physical servers. Integrate renewable energy sources like solar, wind, or hydroelectric power, and consider on-site systems or renewable energy credits (RECs). Implement energy management software and DCIM tools for real-time monitoring. Adopt sustainable practices such as recycling electronic waste, using eco-friendly materials, and conserving water. Conduct regular energy audits and benchmark against industry standards. Collaborate with technology partners and participate in industry initiatives. Educate employees and stakeholders on sustainability. These strategies will help your data center meet sustainability goals and manage rising energy demands.

Maximizing data center uptime is crucial for continuous operations. Implement redundancy measures like N+1, N+2, or 2N for power, cooling, and network systems. Invest in high-quality UPS and backup generators and regularly maintain and test them. Use DCIM software for real-time monitoring and proactive maintenance. Ensure robust physical and cybersecurity with multi-layered protocols and continuous monitoring. Develop and update a disaster recovery and business continuity plan, including data backup and system restoration. Train staff and conduct regular drills. Optimize cooling with hot and cold aisle containment and liquid cooling. Stay updated on industry best practices and technological advancements. These strategies will help to ensure data center uptime and reliable operations.

Lowering data center cooling costs involves both capital expenditures (CapEx) and operational expenditures (OpEx). For CapEx, invest in energy-efficient cooling systems like liquid cooling, advanced data center HVAC systems, and free cooling techniques. Modular data centers, hot aisle/cold aisle containment, raised floor systems, and energy-efficient building designs also help. On the OpEx side, regular maintenance, optimized temperature settings, energy management systems, virtualization, and advanced monitoring tools improve efficiency. Renewable energy sources can offset costs. Combining strategies like choosing cooler climates, using energy-efficient IT equipment, upgrading cooling systems, and training staff on best practices ensures optimal operation. These approaches can significantly reduce cooling costs while maintaining performance and reliability.

You cannot future-proof your data center, but you can prepare by designing a scalable infrastructure with modular components for easy upgrades. Invest in energy-efficient, high-performance hardware and advanced cooling solutions like liquid cooling or free cooling. Use virtualization and cloud technologies for better resource utilization and scalability. Implement software-defined data center (SDDC) principles for automated resource management. Ensure robust cybersecurity with multi-layered protocols and continuous monitoring. Plan for disaster recovery and business continuity. Regularly update infrastructure, stay informed on industry trends, and collaborate with technology partners. Adopt sustainable practices, such as using renewable energy. These steps will help to keep your data center adaptable, efficient, and secure.

Connect with an expert.

Still not sure which solution is right for you? Connect with a Trane expert.

Prefer to chat with someone at your local Trane office?

Opt-in and get the latest data center news

Stay informed on the latest trends and solutions to mitigate your challenges including waste removal, heat reuse, energy storage, noise pollution and more.

Subscribe