Glossary
Free Cooling
Learn what free cooling is and how it can help your organization save money and improve its sustainability.
Quick Facts
- Industry
- Data Centers
Selecting a language changes the language and content on the Trane site.
ComfortSite Login
Trane ComfortSite is an extranet site designed to save you time. With your secure login, you can:
Trane Cloud
Trane Connect is now Trane Cloud—your secure, digital foundation for remotely monitoring and managing building systems, while bringing together insights, applications, and future innovations in one unified experience.
Latin America
Europe
Asia Pacific
Glossary
Learn what free cooling is and how it can help your organization save money and improve its sustainability.
Quick Facts
Free Cooling (also known as economizing) is an energy-efficient HVAC method that uses naturally cool outdoor air instead of mechanical refrigeration to provide cooling for a building or process. When ambient outdoor temperatures are lower than the air or water returning from the building, the system bypasses the energy-intensive mechanical cooling cycle and uses the free outdoor conditions to reject heat.
Free cooling leverages the temperature differential between the outdoors and the building's internal load. Trane systems typically utilize one of two primary methods:
1. Air-Side Free Cooling (Air-Side Economizer) This method is common in packaged rooftop units and air handling units.
The process:
2. Water-Side Free Cooling (Water-Side Economizer) This method leverages cold outdoor temperatures to cool the building's chilled water loop, reducing or eliminating the need to run the chiller’s compressors. Depending on the system design, this is typically accomplished in one of two ways:
The process:
3. Refrigerant-Side Free Cooling (Refrigerant Economizer) Often utilized on centrifugal chillers, this is another method of free cooling that relies on refrigerant migration rather than diverting the chilled water. When the condenser water from the cooling tower is colder than the chilled water, it naturally condenses the refrigerant. Gravity feeds the liquid refrigerant to the evaporator to cool the chilled water loop, providing cooling capacity without turning on the compressor.
Incorporating free cooling is one way to lower operational costs and improve system reliability.
Free cooling can deliver substantial savings and performance benefits, but the right solution depends on your building's unique load profile, climate zone, and operational needs. Whether you're designing a new facility or retrofitting an existing system, our experts can help you determine if free cooling is the right fit and which technology will maximize your return on investment. Contact your local Trane representative today to discuss economizer options, integrated free cooling chillers, and custom solutions tailored to your facility.
Resources & Insights
Ascend™ ACR Air-Cooled Chiller
Carbon Neutral Data Center Cooling