What Is a Token in AI?
A token is the basic unit of text an AI system processes, and in AI-focused data centers it has become a useful metric for sizing and operating infrastructure. More than just a digital concept, tokens represent the tangible, measurable work product of AI infrastructure, much like kilowatt-hours (kWh) are the measurable output of an electrical system.
When an AI model processes or generates information, it does not read whole words the way humans do. Instead, it breaks text, images, or code down into smaller chunks called tokens.
- A token can be a single character, a punctuation mark, a syllable, a whole word, or part of a word, depending on how the model breaks up text.
- As a rule of thumb, 1 token is roughly equivalent to 0.75 words or about 4 characters of English text.
- For example, the phrase "cooling the earth" might be broken down by an AI model into three or four distinct tokens: "Cool", "ing", " the", " earth."
When we talk about the capacity or speed of an AI model, we measure it in tokens per second (t/s).
Tokens as Measurable Output of the AI Factory
Traditional enterprise data centers have historically acted as digital warehouses, storing, retrieving, and moving data. AI data centers operate differently; they are AI factories with higher token throughput. Higher token throughput generally means more demand on GPUs, networking, power delivery, and thermal management
In an AI factory, raw materials, such as electricity, cooling, and compute power, go in, and a refined product comes out. That product is AI tokens.
Every time a user asks an AI chatbot a question, generates an image, or uses an AI-powered search, the physical infrastructure of the data center must work to manufacture tokens. Because of this, they serve as the vital link connecting digital workloads to the physical, real-world resources required to run them, specifically, the compute, power, cooling, and network infrastructure.
Tokens as a Consideration for Data Center Planning and Design
Understanding tokens is no longer only a concern for software engineers. For data center operators, structural planners, system and architectural designers, and thermal management engineers, tokens have become a critical metric shaping physical design decisions.
Designing for Extreme Thermal Densities
To generate a massive volume of tokens rapidly, AI models rely on specialized, power-hungry processors like GPUs (Graphics Processing Units) and TPUs (Tensor Processing Units).
The physics: Processing billions of tokens requires trillions of calculations per second. This massive compute demand translates directly into high electrical power draw, which in turn generates immense, concentrated heat.
The design implication: Traditional data centers designed for air cooling (averaging 5 to 15 kW per rack) cannot handle the thermal load of AI factories, which can easily exceed 40 to 100+ kW per rack. To keep up with token production, engineers must design physical spaces that accommodate advanced thermal management solutions, such as direct-to-chip liquid cooling and high-efficiency chilled water loops.
Managing Dynamic and Variable Thermal Profiles
Unlike steady-state traditional cloud workloads, token generation is highly dynamic.
The physics: An AI system in its idle state uses minimal power, but the moment a massive LLM is prompted to infer or generate tokens, power consumption and heat generation spike instantly.
The design implication: Thermal management systems must be designed for extreme agility. Cooling infrastructure must react in real-time to the rapid rise and fall of thermal loads as token demand fluctuates, requiring smart flow-control valves, variable-speed chillers, and advanced automation software to maintain safe operating temperatures.
Optimizing Tokens
In an AI factory, operational success is defined by resource efficiency, measured through two critical metrics:
- Tokens per watt: This metric measures how much computational work can be extracted from every unit of electrical power. By optimizing Power Usage Effectiveness (PUE) with high-efficiency cooling, operators can redirect more power directly to the chips, maximizing the facility’s overall token per watt output.
- Cost per token: Ultimately, data center economics are driven by the financial bottom line. Because energy is the single largest operational expense for an AI facility, the efficiency of the cooling infrastructure directly impacts the business cost per tokens generated.
The physics: If a data center's thermal management system is inefficient, a massive portion of the facility's power capacity is wasted on overhead cooling rather than being delivered to the GPUs producing tokens.
The design implication: Improving Data Center Infrastructure Efficiency (DCiE) and PUE is critical. By implementing highly efficient chillers, free cooling, and heat reuse technology, Trane helps data center operators maximize the power envelope allocated to compute. The more efficiently a facility is cooled, the more electrical capacity can be dedicated to generating tokens, directly improving the operator's return on investment (ROI).