Trane Connect is now Trane Cloud—your secure, digital foundation for remotely monitoring and managing building systems, while bringing together insights, applications, and future innovations in one unified experience.
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
Glossary

HVAC

What does HVAC stand for, what are the components, and how is a system's efficiency measured? Learn the basics of HVAC from the experts at Trane Commercial.

modern office building stands among lush green trees
modern office building stands among lush green trees

What Does HVAC Stand For?

HVAC stands for Heating, Ventilation, and Air Conditioning. It includes the essential systems that regulate temperature, humidity, and indoor air quality (IAQ) across a wide variety of commercial and industrial spaces. In today’s buildings, HVAC systems are about more than comfort; they are a critical part of maintaining occupant health, energy efficiency, and compliance with evolving codes and sustainability standards.

Whether you're managing a school campus, hospital, data center, or high-rise office building, a well-designed HVAC system can significantly impact operating costs, emissions targets, and long-term infrastructure performance.

Commercial HVAC System Components

Unlike residential applications, commercial HVAC systems must support higher occupancy rates, larger square footage, and more complex usage needs. Components may include

  • Air Conditioners: Central cooling systems that remove heat and humidity from indoor spaces
  • Heat Pumps: Provide both heating and cooling by transferring heat between indoor and outdoor environments. Increasingly favored for all-electric, low-emission strategies
  • Chillers: Refrigeration systems that cool water or a liquid solution, which is then circulated to cool the air. Essential for large-scale air conditioning systems, providing a central cooling source for multiple zones
  • Furnaces: Fuel-burning units (gas or propane) used where high-output heating is needed
  • Air Handlers: Circulate conditioned air throughout the building, especially in systems using heat pumps or chilled water
  • Boilers: Used in hydronic heating systems, especially in institutional and cooler-climate buildings
  • Geothermal Heat Pumps: Use ground-source energy for ultra-efficient heating and cooling in applicable building footprints
  • Ductwork Systems: Distribute conditioned air across zones. Proper design and sealing are critical for efficiency and air quality
  • Humidity Control Systems: Include integrated humidifiers and dehumidifiers to manage indoor air quality and occupant comfort
  • Building Control Solutions: Allow centralized control, scheduling, remote monitoring, and performance diagnostics across large or multi-zone systems and equipment

HVAC System Efficiency Metrics: What Facility Managers Should Know

HVAC equipment must meet stringent performance and efficiency standards. Understanding the key ratings will help you select systems that balance performance with lifecycle cost savings.

AFUE (Annual Fuel Utilization Efficiency)

Applies to gas furnaces and boilers. Expressed as a percentage, it reflects how much of the fuel’s energy is converted into usable heat. A 97% AFUE means 97% of the fuel heats your building, while 3% is lost.

HSPF2 (Heating Seasonal Performance Factor, version 2)

Used for heat pumps, this rating indicates heating efficiency across a range of outdoor temperatures. The updated HSPF2 standard offers a more accurate reflection of seasonal performance.

EER2 (Energy Efficiency Ratio, version 2)

Measures the energy efficiency of a cooling system at a fixed 95°F temperature. It’s particularly useful for evaluating performance in consistently hot climates or peak-load scenarios.

IEER2 (Integrated Energy Efficiency Ratio, version 2 )

Similar to EER2, but measures the energy efficiency of a cooling system under various load conditions.

BTU (British Thermal Unit)

A measure of heat energy. Systems with higher BTU capacity are required for larger or more complex commercial spaces.

dB(A)

This sound level rating is measured in decibels and indicates how loud a system will be during operation. Important in sound-sensitive environments like classrooms, offices, and healthcare.

Types of Commercial HVAC Systems

The type of HVAC system best suited to your facility will depend on building size, layout, usage, local climate, and energy goals. Common commercial system types include the following:

  • Split Systems: Paired indoor and outdoor units—ideal for small buildings or zoned areas. These can include combinations of heat pumps, AC units, air handlers, and furnaces.
  • Packaged Systems: Heating and cooling components are housed in a single rooftop or mechanical room unit. These streamline installation and reduce space needs.
  • Dual Fuel (Hybrid) Systems: Combine an electric heat pump with a gas furnace for optimized heating performance in varying temperatures. The system selects the most efficient heating source based on outdoor conditions.
  • Ductless Mini-Split Systems: Flexible solutions for renovations, additions, or zones without ductwork. Multi-zone configurations allow individualized control for different rooms or building wings.
  • Centralized Systems (Chillers + Boilers): Used in large commercial and institutional buildings, these systems offer high-capacity climate control with integrated air handlers and distribution systems.
  • Geothermal Systems: A high-efficiency solution for buildings with the right physical footprint. Offers low lifecycle cost and reduced emissions.

Codes and Standards for Commercial HVAC

HVAC systems in commercial buildings must meet local, state, and national codes, including:

  • International Mechanical Code (IMC) and International Energy Conservation Code (IECC)
  • ASHRAE standards for energy efficiency, indoor air quality, and system design
  • AHRI performance certification for HVAC equipment
  • EPA and DOE regulations on refrigerants, efficiency, and emissions
  • State-level amendments and decarbonization mandates (e.g., electrification codes, building benchmarking requirements)

Compliance not only ensures occupant safety and regulatory alignment; it also supports ESG reporting, tax incentives, and resilience planning.

Planning the Right HVAC System for Your Facility

Every building is unique. The right HVAC system is determined by

  • Building size and layout
  • Occupant needs and air quality requirements
  • Climate zone
  • Budget and utility incentives
  • Sustainability and electrification targets
  • Future readiness and maintenance strategy

Working with a qualified HVAC engineer or commercial contractor ensures that your system is appropriately sized, energy efficient, and code-compliant.

Why Trane Commercial HVAC?

Since 1913, Trane has led the way in designing and delivering HVAC systems that maximize performance, minimize environmental impact, and adapt to the evolving needs of commercial spaces. With a proven track record across sectors, including education, government, healthcare, and retail, we bring a systems-based approach to every project, helping you

  • Reduce energy consumption
  • Improve indoor environmental quality (IEQ)
  • Comply with refrigerant transition timelines
  • Access available incentives and funding
  • Meet your sustainability and carbon reduction goals

Looking for support with your next HVAC upgrade or replacement? Contact your local Trane Commercial representative to begin planning your solution.