Interested in learning more?
Contact a Trane Expert to advise you on the development, design, and operations of your new data center
Trane ComfortSite is an extranet site designed to save you time. With your secure login, you can:
This is the login for Trane® Connect™ and other Trane® commercial applications. Trane® Connect™ is our secure, cloud-based customer portal to access your building systems to remotely monitor and manage building systems, and conduct routine maintenance.
Selecting a language changes the language and content on the Trane site.
Latin America
Europe
Asia Pacific
Discover which experts from Trane will be presenting and what topics they will cover at the upcoming ASHRAE Winter Conference and AHR Expo
According to computer scientists, the artificial intelligence (AI) we see today pales in comparison to what it could become.
AI is poised to make tremendous advances in the near- and mid-terms. But a single factor is holding back AI-based technology advancement: Power.
Data centers are scrambling to expand capacity to meet exploding demand primarily due to power-intensive AI applications. But they are hampered by utility companies’ ability to provide sufficient energy. Most data centers were built to handle the needs of cloud computing. But AI is taxing their capacity. AI servers need roughly 10 times the computing power1. They also produce 10 times more heat than cloud servers and require advanced cooling methods such as liquid immersion2.
As a result of AI, industry experts believe that the demand for energy may grow by 85% over the next 15 years, and that key data center markets may not have the energy they need within a mere 3-4 years3.
There’s also a development gap. While it can take a utility company 2-4 years to connect a large customer to the grid, a data center can be built in 18 months4.
Fortunately, there are steps you can take that can help flatten the demand curve and help make your data center development plans more attractive to your utility.
“Stranded capacity” refers to installed assets that can’t be used to support critical operations. A data center’s stranded capacity can be found in its power, space and cooling infrastructure. For example,
Freeing stranded capacity in your data center not only demonstrates to your utility that you are using as much power as you are currently allocated, but it also helps increase your leasing capacity.
While your data center may need 100 MW to operate, that doesn’t mean you’ll need the utility to deliver that much 24 hours a day, 365 days a year. In many areas of the country, a utility may experience a strain on their grid for only 10-15 days of the year. With a strategically designed cooling system, you can show the utility how you’ll help reduce your usage during those peak loads.
To curtail your peak demand loads, you’ll need to be able to “unplug” from the utility for a certain amount of time and still operate. Think of your data center like a laptop computer. It charges while it’s plugged into power, but still runs for a while just on its battery.
Energy storage works the same way. Using one of several available types of storage technologies, you can help save that energy for use when you need to unplug from the grid. This includes approaches such as electrical energy storage, battery storage, mechanical storage, biomass and more. At Trane we can work with you to find the right storage solution based on need and application. Here are two solutions we’re seeing customers put on the top of their consideration list:
Any of the energy storage systems mentioned above can be powered by renewable energy sources, such as wind or solar. Could the energy needed for your new data center be supplemented by solar panels on the roof? Or a small wind turbine? Or geothermal? Remember that you only need to generate enough energy to create power for storage, not to run your entire operation. But demonstrating how you’re going green can help when negotiating with utility companies.
Trane’s proprietary solutions could redefine how you think about developing new data centers and retrofitting your old ones. When looking at the total grid, our proprietary technologies, energy contracts and ITC credits could help reduce the cost of building a new data center. Flattening the power demand curve could help:
Trane experts can advise you on the development, design and operations of your new data center, and help you create an approach to cooling and energy use that can position you favorably with utilities. By working together, we can play a part in fulfilling the potential of AI to help elevate the quality of life across the globe.
* Based on an average of $10-12MM per MW cost for new data centers
Contact a Trane Expert to advise you on the development, design, and operations of your new data center
Enhance your services with Trane Rental: 24/7 support, custom engineering, and reliable equipment to exceed customer expectations and build trust.
E+E Leader honors Trane with three awards for 2025 Top Project and Products.
Blog
Innovation
Data Centers
Enhance your services with Trane Rental: 24/7 support, custom engineering, and reliable equipment to exceed customer expectations and build trust.
E+E Leader honors Trane with three awards for 2025 Top Project and Products.
Enhanced air-cooled chillers bring larger capacity and higher ambient temperature cooling capabilities to mission critical operations, further expanding Trane’s thermal management systems capabilities.