Trane Connect is now Trane Cloud—your secure, digital foundation for remotely monitoring and managing building systems, while bringing together insights, applications, and future innovations in one unified experience.
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
Blog

Published: April 24, 2026

6 Ways Trane Rental Services Supports Data Center Operations

Learn how Trane Rental Services can help data centers maintain uptime, support commissioning, overcome delays, and keep construction and operations running smoothly with rapid, engineered temporary cooling and testing solutions.

Trane Rental Service Unit

Brian Jones

Rental Services Business Development Manager - Data Centers

Quick Facts

Topics
Rental Service • Rental Equipment • Data Centers • Data Centers
Services
Rental Services
Trane Rental Service Unit

Data centers leave no room for error when it comes to cooling.

Whether building a new edge facility, expanding an enterprise site, or commissioning a hyperscale location, maintaining thermal stability is essential to keeping data center projects on track. In fact, power and cooling issues account for nearly 40% of major data center outages, highlighting how critical reliable cooling infrastructure is to operational continuity.

When permanent equipment is delayed or unexpected challenges arise, temporary chillers or load bank rentals provide critical support, helping teams maintain cooling capacity, continue testing and commissioning activities, and avoid costly schedule disruptions. 

Trane Rental Services has been a trusted leader in  HVAC equipment rental for over 30 years across all industries. Today, owners and contractors increasingly turn to Trane for engineered temporary power and cooling solutions designed specifically for data center environments. 

Below are six ways our data center rental solutions support reliable hyperscale and colocation facility construction and operation. 

1. Rapid Deployment That Protects Data Center Project Schedules 

Data center projects move fast, often going from site preparation to energized equipment in less than two years, all while requirements continue to evolve. 

Mechanical equipment deliveries don’t always align with fast-moving construction timelines. Electrical rooms and IT racks can show up long before permanent chillers. 

Temporary power and cooling solutions help bridge that gap. 

Rental chillers (air-cooled or water-cooled), pumps, hoses, and power distribution can be delivered and commissioned quickly as a coordinated system, helping teams:

  • Support white space buildouts 
  • Enable early IT deployment 
  • Manage chip-dense rack retrofits 
  • Navigate seasonal temperature swings during enclosure completion 

Maintaining cooling continuity helps control costs, avoid bottlenecks, and keep milestones intact. Industry analyses show that even a single month of delay on a 60 MW data center project can cost developers up to $14 million in lost revenue. 

2. Engineered Data Center Cooling Sized to Real IT Loads 

Data center cooling is not passive or hands-off. Undersized systems risk equipment protection. Oversized systems can create instability and inefficiency. 

Trane Rental Services’ engineers specify each temporary solution based on actual IT loads, redundancy requirements, and construction phases. We commonly support:

  • Commissioning and load testing 
  • Phased pod deployments 
  • Planned mechanical outages 

By modeling expected heat loads and environmental conditions, temporary cooling systems operate as a seamless extension of the permanent plant, not a workaround. 

3. Safer, Faster Level 3 Commissioning with Trane Ascend™ Heat Pump Chillers 

Level 3 commissioning (Startup & Site Acceptance Testing) requires heating capacity to validate hydronic loops and plant sequences. Traditionally, this has meant deploying boilers, which can introduce additional setup time, safety considerations, and higher energy use. 

The Trane Ascend®™ heat pump chiller offers an alternative. 

Trane Ascend®™ heat pump chillers:

  • Provide heating without steam or high-temperature boiler risk 
  • Install faster than traditional boiler systems 
  • Improve energy efficiency 
  • Utilize lower-GWP R-454B refrigerant 
  • Operate similarly to permanent chiller systems, minimizing technician learning curves 

Because our Ascend chillers function like the equipment they’re validating, commissioning teams can move quickly while maintaining precision and control. 

4. Reliable Rental Load Banks for CDU and Chiller Commissioning 

CDU and chiller commissioning requires stable, predictable heat loads to validate performance. Without a controlled false load, confirming CDU and chiller response becomes difficult, often delaying turnover. 

Rental load banks, including water-cooled load banks for hydronic systems, allow teams to:

  • Simulate IT heat loads before hardware installation 
  • Validate performance at partial and peak load 
  • Confirm control sequencing under dynamic conditions 

By working closely with your team, Trane experts help ensure the facility meets requirements from day one, reducing risk and improving the chances of finishing on time and on budget. Strong commissioning practices also support lower operating costs, improved efficiency, and greater uptime. 

5. Data Center Contingency Planning: Redundancy and Resilience During Critical Events 

Even well-designed facilities require operational safeguards. Temporary data center cooling is frequently used to support operations during:

  • Emergency cooling failures 
  • Planned equipment upgrades 
  • Seasonal demand spikes 

When uptime is critical, the reliability of temporary solutions matters just as much as the speed of deployment. Trane Rental Services provides engineered rental systems designed for all types of data center environments, backed by proven equipment, experienced technicians, and responsive service support. 

A rental chiller paired with temporary generators can establish an independent cooling backbone, helping protect uptime, maintain service-level agreements, and provide confidence that operations will continue uninterrupted, even during unexpected events. 

6. Lifecycle Support Beyond Initial Construction 

Temporary cooling plays a role far beyond startup. As data centers expand, modernize, and reconfigure white space, rental solutions provide flexibility without sacrificing uptime. 

We routinely support:

  • Pod-by-pod expansions
  • Equipment and controls upgrades
  • Capacity testing for new tenants
  • Infrastructure modernization

Data center temporary power and cooling solutions enable progress while permanent systems evolve, supporting operational continuity and sustainability goals while keeping your hyperscale or colocation facility future ready.

A Reliable Collaboration for Data Center Cooling

Thermal management is the backbone of data center uptime. From construction and commissioning to upgrades and emergency response, engineered data center rental solutions help protect uptime, performance, and schedule integrity.

If your project requires temporary cooling, power, or load testing support, Trane Rental Services delivers the expertise and equipment to keep your facility moving forward with confidence.