CONTACT A TRANE EXPERT

On-site Training

Commercial Rooftop Burner Service

  • 3 Days
  • 2.2 CEU's

 

This course covers the operation and setup of the gas burners used in the following Trane Commercial Rooftop Units (RTU): Precedent™ 3 to 10 tons, Voyager™ 12.5 to 50 tons, IntelliPak® I 20 to 130 tons, and IntelliPak II 90 to 162 tons. Centering on lab exercises, the service technician will be introduced to the various burners currently used in Trane units from a setup and service perspective. Classroom lecture and exercises will support the hands-on labs. This course applies to new system startup as well as existing buildings.



The lab exercises are designed around several working natural gas burners in our La Crosse, Wisconsin, training lab including the multi-stage and modulating burners used on commercial rooftop units of 3 to 162 tons. During the lab exercises, students will use the various tools needed to set up and service each burner type. Each student has the opportunity to go through the hands-on exercises as well as to observe other students.

 


An early bird discount of 10% off tuition will be given when you register more than 60 days prior to the start date. We also have a package program where you can save up to 40% off tuition of multiple courses! Visit our website for more details at www.trane.com/traneuniversity.

Locations & Dates