We use cookies to enhance your experience on our website. By clicking '' or by continuing to use our website, you are agreeing to our use of cookies. You can change your cookie settings at any time.

What Is a Hydronic Heating and Cooling System?

By Anne Fonda

A residential hydronic heating and cooling system heats or cools a space using water. There are multiple mechanical systems that can provide the energy: air to water heat pumps (AWHPs), boilers, and geothermal systems. 

The water is heated or cooled and then sent into a radiator system or radiant flooring tubes to heat or cool your home. It is also sometimes called a radiant heating and cooling (RHC) system. 

Unlike a traditional forced-air HVAC system, a hydronic heating and cooling system does not utilize ductwork. And unlike a traditional hydronic heating system like a boiler, a hydronic heat pump system will heat your home in the winter, but it will also cool your home in the summer. This makes it a great option if you need to replace your boiler system. It allows you to remove unsightly window AC units or portable air conditioners. 

– Jennie Bergman, Portfolio Leader, Residential Package Units & Light Commercial Unitary 

A hydronic heating and cooling system is highly energy efficient and can also be incorporated into your new home construction, providing both radiant floor heating and radiant cooling.  

While it’s a relatively new concept for U.S. homeowners, hydronic heating is very common in Europe, and hydronic cooling is growing in popularity. HRC systems are very common in U.S. commercial buildings. Studies show that RHC systems can enhance comfort and energy efficiency in sustainable buildings. Most research so far has involved commercial applications, but it is expected that residential applications will see similar benefits. 

Heating SystemWhat You Put InWhat You Get OutHow It Works
Old Boiler (Oil or Gas)$1.00 of fuel70¢ to 80¢Up to 30¢ escapes straight out of the exhaust pipe as smoke and waste gas.
High-Efficiency Modern Boiler$1.00 of fuel90¢ to 95¢ of heat Squeezes almost all the heat out of the fuel, but still loses a small amount up the chimney. 
Air to Water Heat Pump$1.00 of electricity$3.00 to $4.00 of heatUses that $1.00 of power like a delivery truck to gather $3.00+ worth of free renewable warmth from the outdoor air.

Block: Spacer – Responsive

Small Viewport: pb-4
Medium Viewport: pb-6
Large Viewport: pb-6


Anne Fonda, Content Writer

LinkedIn

A Content Writer with Trane Technologies, Anne Fonda researches topics and writes for Trane® and associated residential HVAC brands. She works in collaboration with Trane Technologies subject matter experts, offering easy-to-understand, informative content on complex topics. Her goal is to help consumers make informed decisions on the products and services they need.

She has written for HVAC and other service provider websites for over 16 years. Before transitioning to web content writing, Anne had a 14-year stint as an award-winning journalist. She graduated cum laude from the University of Missouri-Columbia School of Journalism.

When she’s not working, Anne enjoys playing word games, reading, gardening, spending time with family, and visiting gardens and museums.

Expert review by Jennie Bergman, Portfolio Leader, Residential Package Units & Light Commercial Unitary

 

Contact a local dealer

Dealers can answer questions, help you find the right products for your home, and repair your system.

We’re here to help

Connect with our Customer Care team about your products, warranties, and dealer concerns.

Available Monday – Friday from 7am to 5pm CST

1-833-298-3493

A phone

What do you need help with?