We use cookies to enhance your experience on our website. By clicking '' or by continuing to use our website, you are agreeing to our use of cookies. You can change your cookie settings at any time.

What is an Air to Water Heat Pump (AWHP)?

By Anne Fonda

An air to water heat pump (AWHP) is a heat pump that uses water to heat and cool your home. It’s a heating and cooling system that extracts heat from the air, and transfers heat into water or a water-glycol mixture. Because it uses water, it is also known as a hydronic heating and cooling system. 

While still emerging as a heating and cooling solution residential applications in the United States, AWHP systems are quite common in Europe as well as commercial buildings in the U.S. 

How do air to water heat pump systems work? 

Much like an air source heat pump, an air to water heat pump extracts heat from the air. Using the refrigeration cycle, it heats or cools water in the outdoor unit and distributes it through connected water lines to in-floor radiant tubes, fin tube baseboards, or radiators throughout the home.   

When it’s cold out and you turn on the heat, the hydronic heat pump heats the water; when it’s hot out and you need to cool things down, it reverses the refrigeration process, turning into a chiller that sends cold water through the radiant system or fan coil units for whole-house cooling and dehumidification.   

The system includes:  

  • Outdoor hydronic heat pump  
  • Indoor thermostat – the brains of the system  
  • Water storage tank  
  • Radiant distribution system (radiant flooring tubes, radiators, fin tube baseboards)  
  • Fan coil units (for cooling)   

Where are air to water heat pump systems best suited? 

There are two main scenarios: you need to replace an aging and inefficient boiler system, or you are building a new home and you desire premiere comfort through radiant floor heating (and cooling). AWHP systems do not need ductwork, making them a great home comfort solution for older homes as well as energy-efficient new construction or renovations. 

– Jennie Bergman, Portfolio Leader, Residential Package Units & Light Commercial Unitary 

Can an air to water heat pump cool my home? 

Yes. As we mentioned above, an AWHP system can heat your home in cold weather and cool your home in warm to hot weather. This is part of what makes it such a great alternative to boiler replacement. 

Can it supply my hot water, too?

– Jennie Bergman, Portfolio Leader, Residential Package Units & Light Commercial Unitary 

How efficient are air to water heat pumps compared to a boiler? 

– Jennie Bergman, Portfolio Leader, Residential Package Units & Light Commercial Unitary 

How much does an air to water heat pump installation cost? 

Your cost will vary greatly based on several factors, including: 

  • The size of your home 
  • If the AWHP system is replacing a boiler in a retrofit or if this is new construction 
  • If you need new radiators or fin tube baseboards Other factors specific to your home 

“An air to water heat pump generally costs more to purchase and install upfront than a standard replacement boiler. However, because it replaces three separate appliances (heating boiler, central air conditioner, and domestic water heater) and operates at 300%+ efficiency, the long-term energy savings and available electrification incentives significantly shorten the payback window.” 

When looking solely at heating quotes, heat pumps can look more expensive on paper. To make it an apples-to-apples comparison, homeowners should view it as a bundled investment: 

If You Buy SeparatelyIf You Choose Air to Water…
New High-Efficiency Gas/Oil Boiler ~$11,000 One Air to Water Monobloc/Split Unit
New Central AC/Mini-Split System ~$8,000 Integrated indoor hydronic fan coils/radiant cooling
Standalone Water Heater ~$2,500 Dedicated indirect hot water tank tied to the heat pump
Combined Total ~$21,500* Combined Total: ~$18,000-$24,000 (before any rebates)

*These are rough estimates of equipment and installation costs for these components. Prices will vary by contractor and equipment brand. 


Anne Fonda, Content Writer

LinkedIn

A Content Writer with Trane Technologies, Anne Fonda researches topics and writes for Trane® and associated residential HVAC brands. She works in collaboration with Trane Technologies subject matter experts, offering easy-to-understand, informative content on complex topics. Her goal is to help consumers make informed decisions on the products and services they need.

She has written for HVAC and other service provider websites for over 16 years. Before transitioning to web content writing, Anne had a 14-year stint as an award-winning journalist. She graduated cum laude from the University of Missouri-Columbia School of Journalism.

When she’s not working, Anne enjoys playing word games, reading, gardening, spending time with family, and visiting gardens and museums.

Expert review by Jennie Bergman, Portfolio Leader, Residential Package Units & Light Commercial Unitary

 

Contact a local dealer

Dealers can answer questions, help you find the right products for your home, and repair your system.

We’re here to help

Connect with our Customer Care team about your products, warranties, and dealer concerns.

Available Monday – Friday from 7am to 5pm CST

1-833-298-3493

A phone

What do you need help with?