Glossary
Liquid Cooling
Learn about liquid cooling and discover why it's an efficient way to cool your buildings, including data centers.
Quick Facts
- Industry
- Data Centers
Selecting a language changes the language and content on the Trane site.
ComfortSite Login
Trane ComfortSite is an extranet site designed to save you time. With your secure login, you can:
Trane Cloud
Trane Connect is now Trane Cloud—your secure, digital foundation for remotely monitoring and managing building systems, while bringing together insights, applications, and future innovations in one unified experience.
Latin America
Europe
Asia Pacific
Glossary
Learn about liquid cooling and discover why it's an efficient way to cool your buildings, including data centers.
Quick Facts
Liquid cooling is a method of heat removal that involves the circulation of a liquid, typically a 25% propylene glycol mixture, to transfer heat away from graphics processing units (GPUs). The coolant distribution unit (CDU), is often paired with chillers, air handling units, and cooling towers to ensure proper heat removal for the entire data center.
Compared to air cooling, liquid cooling is a more efficient method of heat transfer because the liquids used have a higher heat capacity and thermal conductivity. For example, water can carry 3,500 times more heat than air and has 24 times higher thermal conductivity.
Liquid cooling systems circulate a coolant through a network of pipes, coils, or blocks that come into direct contact with GPUs. The liquid absorbs heat and is then pumped to a heat exchanger (like a radiator or cooling tower) where the heat is dissipated. The cooled liquid then returns to continue the cycle.
Water is commonly used for liquid cooling because it's often readily available and inexpensive. Distilled or deionized water is recommended to reduce the risk of mineral buildup or corrosion. Ethylene glycol and propylene glycol are common additives to water in liquid cooling systems because they can improve freeze protection and corrosion inhibition.
When water is not readily available, as in drier climates or drought-stricken regions, other liquids can be used. Dielectric fluids are useful for immersion cooling when electrical parts are in direct contact with the liquid and are often used for liquid cooling in data centers. Some refrigerants are also compatible with immersion cooling. Talk to your local Trane expert to learn which liquid will fit your needs best.
Liquid cooling is the most efficient choice for data centers, especially when faced with high heat loads, space constraints, or a need for quieter operation. Coolant distribution units work well amongst densely packed servers, where air cooling struggles to keep up with heat generation.
Standard commercial cooling equipment is not sufficient for hyperscale or colocation data centers. Liquid cooling works best in these facilities due to its superior heat absorption and dissipation, which enables higher server densities while improving energy efficiency. By ensuring equipment stays within safe temperature thresholds, liquid cooling helps extend its lifespan, lowering operational costs over the long term.
Resources for Liquid Cooling
Trane Commercial HVAC offers liquid cooling options, including water-cooled chillers and coolant distribution units for a wide range of applications. Contact your local Trane representative to discuss the liquid cooling system that will best fit your organization's requirements.