Trane Connect is now Trane Cloud—your secure, digital foundation for remotely monitoring and managing building systems, while bringing together insights, applications, and future innovations in one unified experience.
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
      • Domestic Hot Water Heat Pump
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
  • Domestic Hot Water Heat Pump
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
Glossary

What Is a Dual-Fuel Heat Pump?

Learn how a dual-fuel heat pump can provide more efficient, reliable heating and cooling year-round.

Precedent Heat Pump Unit

Quick Facts

Products
Heat Pumps • Packaged Rooftop Solutions
Precedent Heat Pump Unit

What Is a Dual-Fuel Heat Pump?

A dual-fuel heat pump, also known as a dual-fuel heat system or hybrid heat pump system, is a packaged rooftop HVAC unit that combines an electric heat pump with a secondary fossil-fuel heating source (typically a gas-fired furnace or gas/propane heat exchanger) and automatic controls that switch between the two heat sources. The system uses the heat pump as the primary heating source for most conditions and automatically transitions to the fossil-fuel heat source when outdoor temperatures, load conditions, or economics make the fuel option preferable.

How Does a Dual-Fuel Heat Pump Work?

Dual-fuel systems intelligently switch between the electric heat pump and the gas furnace to maintain comfort while maximizing energy efficiency. The system's operation is guided by outdoor temperature sensors and a smart thermostat.

During warmer months, the heat pump functions as a standard air conditioner, transferring heat from inside the building to the outside. In milder heating seasons, the heat pump reverses this process, efficiently extracting heat from the outdoor air and moving it indoors.

When the outdoor temperature drops to a point where the heat pump can no longer operate efficiently, the system automatically switches to the gas furnace to provide powerful heating. This seamless transition ensures the building remains comfortably warm even in very cold conditions. Once the outdoor temperature rises again, the system will switch back to the more energy-efficient heat pump.

Benefits of Dual-Fuel Heat Pumps

  • Improved seasonal efficiency: the heat pump is the primary source over much of the heating season, providing a higher seasonal COP (coefficient of performance) and lower electricity use compared with resistive electric heat.
  • Reliable low- and high-capacity heating: the fossil-fuel burner supplies higher heat output at very low outdoor temperatures or during extreme load events, ensuring capacity and faster recovery.
  • Lower operating cost in mixed climates: using the most economical heat source (electric heat pump when efficient; gas when more cost-effective) can reduce fuel costs compared to single-source systems.
  • Reduced peak electrical demand and grid stress: switching to gas during very cold periods reduces building electrical demand at peak times versus relying solely on electric heat.
  • Fuel flexibility and resilience: having both energy sources increases operational resilience during fuel or power price swings and allows facilities to adapt to changing utility rates or on-site generation strategies.
  • Improved occupant comfort and control: staged heat sources maintain stable supply-air and space temperatures and provide faster recovery from setback conditions.
  • Easier rooftop installation and serviceability: packaged units simplify installation and serviceability compared with field-assembled dual-fuel systems.
  • Incentive and decarbonization pathways: in many cases, heat pumps reduce greenhouse gas emissions across the heating season compared to gas-only systems. Dual-fuel units can help owners adopt heat pumps while retaining fuel backup, enabling phased electrification strategies.

Resources for Dual-Fuel Heat Pumps:

  • Trane Packaged Rooftop Units
  • Decarbonize Now: Your Rooftop Unit is How

Trane offers a variety of dual-fuel heat pumps to fit commercial applications, from a small retail store to a large office building. To determine the best rooftop unit for your building, contact your local Trane representative.
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
Privacy Policy English | French 
Terms of Use English | French

All trademarks referenced are the trademarks of their respective owners.

© 2026 Trane. All Rights Reserved.

Trane Technologies