Trane Connect is now Trane Cloud—your secure, digital foundation for remotely monitoring and managing building systems, while bringing together insights, applications, and future innovations in one unified experience.
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
Customer Story & Case Study

How Cogeneration Reduced a Hospital’s Electricity Usage by 50%

Reducing a hospital’s electricity usage by 50%.

Quick Facts

Location
Traverse City, Michigan
Industry
Healthcare
Products
Building Automation Systems • Tracer® Ensemble
Topics
Innovation • Energy, Environmental and Sustainability • Energy Efficiency

Results

  • Large Footprint The hospital occupied 1 million square feet and contained 442 beds
  • ~$1 million rebates applied for through the Inflation Reduction Act (IRA)
  • >50% savings in hospital's electricity bill ($70,000/month)
  • 28% reduction in hospital's carbon footprint

The Challenge

Trane’s comprehensive approach to helping hospitals optimize energy efficiency and meet sustainability goals was showcased recently at Munson Medical Center in Traverse City, Michigan. One of the region’s largest hospitals, the 442-bed facility occupies a total area of some 1 million square feet and serves as the primary referral center for 24 northern Michigan counties.

The Solution

Technology

Cogeneration, also known as combined heat and power (CHP), is an on-site power generation strategy by which the exhaust heat that’s created by the generator—in this case is powered by natural gas—is recovered instead of being released into the air. The heat is then recycled for use in heating and cooling applications.

A highly efficient solution, cogeneration can provide hospitals with a host of benefits, among them greater resiliency during an outage, flexibility and adaptability in power supply management, and significant cost savings.

“Cogeneration is really beneficial for hospitals because they have a great baseload of electrical usage all year round,” said Brian Langerak, Account Manager at Trane. “Plus, they have steam usage all year round as well as hot water usage. The system can run 24/7/365 and produce electricity, steam and hot water and really make a big dent in utility bills.”

Approach

Trane undertook a comprehensive approach to the project using a data-driven strategy that started with a feasibility study to determine if cogeneration could be installed at the Munson Medical Center with an attractive financial rate of return. Once the study proved positive, the project moved into an investment-grade audit, which included engineered drawings and guaranteed maximum pricing from contractors and suppliers. The final proposal was given the green light to move ahead in short order by the Munson Healthcare executives. Rebates of nearly $1 million through the U.S. Inflation Reduction Act (IRA) pushed the project’s IRR above 20%.

Installation of the cogeneration system into the hospital’s main electrical power grid and steam system proceeded smoothly. Throughout the project, the Trane team helped ensure that the work didn’t impact hospital operations or patient care. Once the solution was installed, the Trane team added the cogeneration system to the hospital’s Trane Ensemble building automation system so the facilities team could manage and monitor the system remotely.  The plant currently provides all the hospital’s power, steam and hot water needs. Combined with their existing emergency generators, it’s capable of providing power to their entire campus during an outage. 

The Results

“Cogeneration projects for healthcare are so beneficial they can become cash positive from literally day one,” said Langerak. And indeed, the new cogeneration plant cut the hospital’s electricity bill by more than 50 percent. As a result of the project Munson Medical Center also reduced its carbon footprint by a full 28 percent.

“As far as operational savings go, we’ve seen right around our projected estimated amounts which were $70,000 a month,” said Ed Belanger, Director of Facilities & Plant Operations, Munson Healthcare. “It’s been a good process, very smooth, well communicated. We are pleased with Trane’s holistic approach. We especially appreciate their understanding of available funding resources, leaving us more resources to devote to direct patient care.”

Customer Stories

Learn how we’ve helped other customers.

    • Customer Story & Case Study

    Campbellford Memorial Hospital and Trane

  • Asante_Rogue_Regional_Medical_Center_535x339.jpg
    • Energy Efficiency
    • Customer Story & Case Study

    Asante Rogue Regional Medical Center

    Asante Rogue Regional Medical Center added a fifth chiller and updated controls with Trane, saving nearly $187,000 annually and increasing redundancy and energy efficiency.

  • Senior patient and nurse in hospital
    • Indoor Environmental Quality
    • Customer Story & Case Study

    Jewish Eldercare Centre

    Jewish Eldercare Centre upgraded its HVAC with Trane's geo-exchange system, saving $250,000 annually and improving comfort and reliability for residents.

Help is closer than you think.

Work with dedicated local Trane representatives who can team with you to solve your problems while providing training and insights.

Find Your Trane Rep Contact Us