Trane Connect is now Trane Cloud—your secure, digital foundation for remotely monitoring and managing building systems, while bringing together insights, applications, and future innovations in one unified experience.
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
Blog

Published: May 18, 2026

The ROI of Grid-Ready, Resilient Buildings

Energy Market Ozark Quote
Emily Harris Market Intelligence Specialist - Energy Services

Emily Harris

Energy Market Intelligence Analyst

Energy Market Ozark Quote

Electricity powers nearly every aspect of life, yet the U.S. now experiences more outages than any other developed country.[1] Power disruptions have risen 25% on average over the last decade[2]—and more than 50% in some states over the past four years—raising concerns about power grid stability and the growing risks to homes and businesses.[3]

Power Grid Disruptions Cost Owners $200 Billion Annually

Power outages are estimated to cost building owners over $200 billion annually as a result of downtime, productivity losses, and a range of impacts to building tenants and dependents[4]

For businesses, outages can halt production, spoil inventory, and eliminate critical revenue. For communities, especially vulnerable populations, prolonged outages threaten comfort and access to essential services.

These outages are becoming more frequent, costing communities billions, and are not going to stop anytime soon.

Why Are Power Outages Increasing?

Several factors are straining the grid simultaneously.

Aging Energy Infrastructure
Much of the grid is decades old. Nearly 40% of transformers are beyond their intended lifespan, and over 70% of transmission lines are approaching the end of theirs.[5]

Aging equipment fails more often, contributing to significant economic losses, estimated between $28-$169 billion annually.[6] Further, aging infrastructure is increasingly vulnerable to natural disasters ranging from fallen trees to expansive wildfires.

These costs are shared between utilities and business owners, as increasing maintenance costs lead to increasing electricity rates. Aging energy infrastructure is leading to increasing day-to-day energy costs and economic losses due to power outages.

Extreme Weather
Severe weather is the leading cause of outages. Heat waves, cold snaps, wildfires, hurricanes, and storms increasingly stress an already aging system.

Events like the 2025 nor’easter storm left hundreds of thousands of communities and businesses without power across the Northeastern U.S.[7]. In 2024, Hurricane Helene led to one of the largest power outages in the U.S. in the last decade[8], while heatwaves in Texas left millions without power in the wake of Hurricane Beryl.[9] Events like these show how quickly extreme conditions can overwhelm generation and transmission systems, leaving communities without power.

Growing Demand and Shifting Supply
Electricity demand is surging after years of stability.

Computing, on-shored manufacturing, and electrified industries are shifting and increasing demands on already overloaded electricity systems. At the same time, base-load coal and natural gas plants are retiring faster than they’re being replaced.

Development of cost-effective distributed and renewable energy is essential and continues to see investment[10], but introduces challenges of intermittency, needing sufficient long‑duration storage, grid modernization, and demand-side management to ensure reliability.

How Building Owners Can Protect Assets and Tenants

Addressing operational, technical, and financial resiliency has never been more accessible. By enhancing building infrastructure and systems, owners can optimize asset performance while hardening their operations against the threat of power outages. Every building’s needs are different, but common methods to boost resiliency include:

  • High-efficiency HVAC Equipment and Systems: High efficiency equipment lowers overall energy demand permitting buildings to operate longer and more comfortably with less power. The reduced load on backup power systems helps improve stability and protects building assets, while also reducing load on the electric grid.
  • Smart Building Solutions: Leveraging controls and automation to optimize energy use across building systems helps reduce noncritical loads and ensures essential functions remain prioritized. These technologies can also coordinate with utility systems during periods of grid stress by automatically adjusting setpoints. As a result, buildings can rely less on backup power during outages and reduce exposure to high demand charges on utility bills.
  • Distributed Energy Resources (DERs): DERs like energy storage and solar can supply onsite power when the grid fails, with the potential to keep critical operations running longer. When prioritized to support HVAC systems, DERs can help ensure critical heating and cooling needs are met in the face of a power outage.

Together, these solutions can also boost the affordability of operating a building. By reducing energy consumption, optimizing demand during peak periods, and leveraging on-site power, these solutions lower operating costs while guarding against expensive unplanned outages. Reliable buildings also assist with tenant satisfaction, revenue continuity, and long-term asset value.

Resiliency in Action: New Mexico's Green Energy Project

The Problem: In 2018 New Mexico’s government leaders faced a common dilemma: how to modernize aging buildings in a way that was fiscally sound and environmentally sustainable. At more than 50 years old, 30-plus State-owned buildings in the capital of Santa Fe were uncomfortable for staff and visitors, with inefficient HVAC systems that left them unbearably hot during Southwestern summer heatwaves and cold in the desert winters. The Santa Fe campus’s fragile building infrastructure was no match for the pressure of fluctuating temperatures and weather uncertainty.

The Santa Fe campus’s fragile building infrastructure was no match for the pressure of fluctuating temperatures and weather uncertainty.

The Trane Solution: Modernizing 32 state-owned buildings with ultra-efficient HVAC systems, intelligent building controls and renewable distributed energy resources enhances comfort, accelerates the State’s climate action plans and economic goals.

Not only are the facilities now safe and comfortable for visitors and staff members, the improvements ensure they will stay that way, even in the face of future calamities. If the State loses power during a wildfire, for example, a back-up energy supply kicks in, thanks to on-site energy storage.

A Practical Path Towards Energy Resilience

While some investments can demand extensive coordination and execution time, owners can strengthen energy resilience today. With Trane, owners are adopting flexible turnkey resiliency solutions to boost building and system reliability with limited impact on their existing operations. 

How Trane Can Help

  • High‑Efficiency Environmental Technologies: Reduce demand and maintain comfort during grid events through reliable HVAC and lighting systems.
  • Advanced Building Automations: Improved performance and energy use with intelligent, real‑time integrated controls and flexible load management.
  • Energy Storage & On-site Generation: Supply backup power and lower demand charges while enabling energy independence by producing and storing power on-site.
  • Turnkey Modernization: Deliver end-to-end solution design, financing, installation and commissioning with one hand to shake throughout the process.
  • Ongoing Optimization: Provide ongoing building and systems monitoring, maintenance and optimization support.

Let’s build a resiliency plan around your reality. Request a quick assessment to understand your risks, options, and potential savings.

 

[1] https://www.pew.org/en/research-and-analysis/articles/2025/04/03/the-us-power-grid-needs-modernizing-distributed-energy-resources-are-one-answer 

[2] Data from 2014-2024

[3] Annual Electric Power Industry Report, Form EIA-861 detailed data files - U.S. Energy Information Administration (EIA)   

[4] Department of Energy Report Explores U.S. Advanced Small Modular Reactors to Boost Grid Resiliency | Department of Energy

[5] https://wjarr.com/sites/default/files/WJARR-2023-1723.pdf

[6] https://wjarr.com/sites/default/files/WJARR-2023-1723.pdf  

[7] Northeast Storm Knocks Out Power, Cancels Over 10,000 Flights Across US - Bloomberg

[8] Hurricanes in 2024 led to the most hours without power in the United States in 10 years - U.S. Energy Information Administration (EIA)

[9] Dangerous heat threatens millions of Texans without power for days in largest outage in utility’s history | CNN

[10] Solar power generation drives electricity generation growth over the next two years - U.S. Energy Information Administration (EIA)