HVAC Troubleshooting

Follow our interactive troubleshooting guide to find answers to your system’s problems. Choose from a selection of common HVAC issues or pick your product for help with fixes you can try yourself.

HVAC Air Handler Overflow Switch

When your air conditioner or heat pump is cooling your home, that cooling process produces condensation. Your air handler is equipped with a drainage system to keep the water droplets flowing down and away from the indoor unit.

The water eventually makes its way to the condensate drain pan and then to the condensate drain line that carries the water outside. But occasionally, the drain line or drain pan can become clogged with dirt, debris, mold growth, or even spider webs.

This can cause water to flow onto the floor of your attic, basement, or utility closet. If not detected, water damage and mold growth can occur.

A condensate switch can prevent water overflow and water damage.

How does the condensate overflow switch work?

If the switch detects a potential condensate overflow issue, it will shut the outdoor compressor and condenser fan down. It will also shut down the supply fan. So, if you have a condensate drain switch, and your air conditioner or heat pump suddenly shuts off in the heat of the day, a clogged condensate line or clogged condensate pan may be to blame.

There are two types of condensate overflow safety switches.

HVAC float switch

An air handler float switch works like a miniature sump pump float switch. When the condensate level reaches the trip point, it triggers an action. In the case of a sump pump, it starts pumping water out of your home. In the case of the condensate float switch, it signals the HVAC system to shut down so as not to produce any more condensation.

Sensor switch

A sensor switch shuts the system down as soon as it detects a few drops of water. This prevents any water overflow or water damage. The switch is installed on the inside or outside of the condensate drain pan.

Do all air handlers have a condensate overflow switch?

No, they do not. This is another reason why regular HVAC maintenance is so important. During a routine visit, an HVAC technician will check the condensate drain line and drain pan for clogs or cracks and replace parts as necessary.

Trane sells a drain pan overflow switch as an accessory. You can have it installed at the time of a new HVAC installation or during a repair or maintenance visit.

Prevent problems with regular maintenance

Did you have condensate overflow in your basement, crawl space, or utility closet because you don’t have an overflow switch? Consider having your HVAC technician install one when they come to clean or replace the drain line and drain pan. It can prevent water damage in the future.

An important part of keeping your AC unit or heat pump running is keeping the condensate line clear, which can be done with regular HVAC maintenance. Schedule AC maintenance every spring and heat pump maintenance in the spring and fall. During a professional maintenance visit, the technician will check the outside unit as well as the air handler blower motor, evaporator coil, and more.


Anne Fonda, Content Writer at Trane Technologies

A Content Writer with Trane Technologies, Anne Fonda researches topics and writes for Trane® and associated residential HVAC brands. She works in collaboration with Trane Technologies subject matter experts, offering easy-to-understand, informative content on complex topics. Her goal is to help consumers make informed decisions on the products and services they need.

She has written for HVAC and other service provider websites for over 16 years. Before transitioning to web content writing, Anne had a 14-year stint as an award-winning journalist. She graduated cum laude from the University of Missouri-Columbia School of Journalism. When she’s not working, Anne enjoys playing word games, reading, gardening, spending time with family, and visiting gardens and museums.

Expert review by Erica Harrison, Product Manager, Air Handlers

Is your HVAC system still experiencing issues?

Your local Trane dealer can help.

Maintenance Tips

A healthy HVAC system can last longer and save money. Maintain your system with these tips.

Owner’s Manual

Learn more about your product, like its technical specs and innovative technology.

Warranty & Registration

After getting a new system, be sure to protect it with a warranty.

Contact a local dealer

Dealers can answer questions, help you find the right products for your home, and repair your system.

We’re here to help

Connect with our Customer Care team about your products, warranties, and dealer concerns.

Available Monday – Friday from 7am to 5pm CST

1-833-298-3493

A phone