What does Central AC Replacement Cost?
Key takeaways:
- Nationally, replacing a central AC unit can cost from $3,900 for a basic base unit to $13,500 on the high end.
- More efficient outdoor units with a higher SEER2 and more speeds will cost more.
- Higher capacity units, such as a 5-ton AC unit, will cost more than a 2-ton AC unit.
- In 2026, Trane AC unit replacement costs nationally average from $6,958-$13,418 installed.
- For precise numbers for your home, get 3 detailed quotes.
By Anne Fonda
You depend on your central air conditioning system to reliably cool your home. But if the cooling is sub-par and AC repair costs are getting more expensive, you’re smart to be researching what it will cost to replace your air conditioner, and what factors influence that cost.
What are some air conditioner replacement cost factors?
In those key takeaways, there’s a big dollar range. That’s because of numerous factors affecting the cost to replace an AC unit.
These include:
- Brand
- Capacity
- SEER2 rating
- Number of stages or speeds
- Local labor costs
- The HVAC company you choose
Let’s dive into these factors and how they affect your AC unit replacement cost.
1. Brand
No matter what you’re buying, the brand will always affect pricing. Whether it’s a purchase as big as a new car or something like deciding where you shop for groceries, there are budget brands, middle-of-the-road brands, and premium brands.
But as you’ve no doubt learned by now, you get what you pay for. Sometimes, those budget items don’t last as long (or taste good), and you have to repair or replace them sooner, whereas a quality brand can last much longer, bring more enjoyment, and save you money in the long run.
Trane is a premium HVAC brand. We use cutting-edge technology, long-lasting components, and put our HVAC equipment through strenuous testing to help ensure you get a new air conditioner that will stand the test of time. That premium quality comes at a higher price than builder-grade brands.
Our HVAC equipment is known for its quality and durability. It’s part of what earned us the title of America’s Most Trusted® HVAC Brand for 12 years in a row.
2. Capacity needed for your home size
A central air conditioner’s cooling capacity is measured in tons. In general, units range in size from 2 tons to 5 tons, with smaller capacity units being suited for smaller homes and larger capacity units being suited for larger homes.
It’s important that your replacement unit be sized properly for your home via a load calculation. Both oversized and undersized units can cause comfort issues and unnecessarily high energy bills.
“Beware of HVAC companies that don’t perform load calculations and rely either on very basic square footage rules of thumb or just want to replace your system with whatever you currently have. Those are usually signs that you should find a better company.”
- Mark Woodruff, Senior Product Manager, Air Conditioners

3. SEER2 efficiency rating
SEER2 stands for Seasonal Energy Efficiency Ratio. It measures an air conditioner’s (or heat pump’s) cooling efficiency average over the entire cooling season. The higher the SEER2 rating, the more efficient the air conditioning unit is at cooling.
A higher SEER2 can be a big deal if you live in a hot and humid area vs an area with mild summers with low humidity.
Our Pricing Guide lays out the cost of Trane AC units with varying SEER2 ratings.
4. Number of stages or speeds
Central air conditioners come in several types: single-stage, two-stage, multi-speed, and variable speed.
Single-stage systems are either ‘On’ or ‘Off’. That means they either run 100% full power or they are off. These units are the cheapest upfront, but will cost more to operate in the long-term.
Two-stage systems are more efficient than single-stage units, and will have a high speed and a low speed (usually 100% and 70% respectively), or be off.
Multi-speed systems are a newer design and straddle the gap between traditional two-stage systems and variable speed. They offer better efficiency than single or two-stage systems but are simpler than variable speed systems. They cost more than 1-or 2-stage units, but less than a variable speed unit.
Variable speed air conditioners are the most efficient as they can vary their output and draw the least amount of power required to maintain your desired temperature. This means they will run for longer at lower speeds for optimal comfort. They cost the most upfront, but can help you save energy for years to come.
“The number of speeds or stages typically translates to better energy efficiency and better comfort… so the more variability or number of stages, the more efficient the equipment will operate and the better temperature and humidity control the system can deliver to your home.”
- Mark Woodruff, Senior Product Manager, Air Conditioners
“Variable speed systems are quieter (both inside and outside the house), more efficient, offer better temperature and humidity control, and have the greatest onboard diagnostics data to monitor system performance and reliability. It is up to the homeowner to decide how important those features are to them,” Woodruff continued
5. Local labor costs
If your home is in a high-cost-of-living (HCOL) area, your new air conditioner will come with a higher price tag than if you lived in a low-cost-of-living (LCOL) area. That’s because HVAC companies in your area need to pay their HVAC technicians a reasonable wage to keep the best talent.
Those higher labor and operating costs will get passed on to you, the homeowner. It’s the same way a car dealer in California will have a higher dealer markup than a car dealer in Iowa, for instance. Higher demand and the local cost of living impact your final costs.
6. The HVAC contractor you choose
Some companies will have lower AC replacement cost estimates than others. Part of this will depend on the brand they are recommending, but it can also be affected by their business operating model.
Are they a small mom-and-pop shop run out of the owner’s home, or are they a large company with multiple locations, a fleet of vans, and a big marketing budget? The overhead costs may impact the quote(s) they give you.
Read our blog on how to find the best HVAC service near me for some tips on selecting the right HVAC contractor. Because even the best HVAC system won’t live up to its potential if it is installed improperly. A faulty installation can lead to discomfort, early repairs, and early system failure.
Do I really need to replace my furnace at the same time?
Maybe. If your furnace is relatively new and your HVAC company can find you a compatible air conditioner, you might be able to get away with just replacing the outdoor AC unit and the indoor coil.
However, if your furnace is older, it might be more cost-effective and provide better comfort and efficiency year-round if you replace the entire HVAC system at once.
“My advice to anyone who may have an aging system that requires frequent repairs is to consider replacing the whole system versus just one component. Typically, with an older system, the technology has become obsolete, and new parts are not completely compatible with older systems.”
-Kimberly Sexton, Senior Systems Engineer, Trane Technologies

How can HVAC financing help me get the air conditioning system I need?
Getting a new air conditioner or new HVAC system doesn’t need to break the bank. While we get that the upfront cost of AC replacement can cause sticker shock, if you finance your new HVAC system, you can break it down into easy monthly payments.
Explore HVAC financing with your local Trane dealer.
How much does it cost to replace an AC unit in your area?
The best way to find out is to get multiple quotes. Your local Trane dealer (or dealers) will ask you about any heating and cooling issues you currently have, perform a load calculation and other system reviews, and then provide you with a quote. They may quote several different systems at different SEER2 levels to give you a side-by-side comparison. They are also happy to discuss their recommendations and answer any questions you may have.
Anne Fonda, Content Writer
A Content Writer with Trane Technologies, Anne Fonda researches topics and writes for Trane® and associated residential HVAC brands. She works in collaboration with Trane Technologies subject matter experts, offering easy-to-understand, informative content on complex topics. Her goal is to help consumers make informed decisions on the products and services they need.
She has written for HVAC and other service provider websites for over 16 years. Before transitioning to web content writing, Anne had a 14-year stint as an award-winning journalist. She graduated cum laude from the University of Missouri-Columbia School of Journalism.
When she’s not working, Anne enjoys playing word games, reading, gardening, spending time with family, and visiting gardens and museums.
Expert review by Mark Woodruff, Senior Product Manager, Air Conditioners