We use cookies to enhance your experience on our website. By clicking '' or by continuing to use our website, you are agreeing to our use of cookies. You can change your cookie settings at any time.

Traditional Thermostats

Choose how your system heats and cools your space with helpful controls. Set your desired temperature, and let your thermostat do the work to keep your home comfortable.

What to look for: cooling speeds, heating speeds, programmability

Find a Local Pro
smart thermostats product category
Showing results for
There are no products that meet this criteria; please broaden your filters to see products

Support Resources

Find guides to help you set up and use your smart thermostat and Trane Home account.

Getting Started Guide

Learn helpful HVAC tips and tricks before you purchase your system.

Owner’s Manuals

Learn more about your product, like its technical specs and innovative technology.

Get helpful HVAC tips in our newsletter

Sign up for our email newsletter to learn helpful HVAC tips and tricks before your purchase your system.

Why choose a Trane traditional thermostat 

Our traditional thermostats include basic programmable thermostats and entry-level non-programmable thermostats. Like every Trane product, reliability is built in. You might choose one of these thermostats if you feel like you don’t want or need all of the extra options that come with smart thermostats.  

Ease of use 

Traditional thermostats are easy to use. Non-programmable thermostats are the simplest. You set the indoor temperature you want, and it stays there until you change it. Programmable thermostats have an intuitive interface that allows you to set a schedule for different times of day and days of the week.  

Setting a lower or higher temperature (depending on the season) for while you’re away can help you save money on your energy bills. 

Digital thermostats improve visibility of important data 

If you grew up with (or still have!) the old circular dial thermostat with tiny numbers or a toggle switch thermostat with equally tiny numbers, you’ll appreciate the digital display of our newer traditional thermostats.  

The inside temperature is displayed large enough to be seen easily. Depending on the unit, you may have a touchscreen or buttons to push to raise or lower the temperature. Most units also display the time, and some can display the outdoor temperature or indoor humidity level. 

Compatibility with single-stage and two-stage systems 

If you have a single-stage or two-stage HVAC system, our traditional thermostats are compatible.  

Traditional Thermostat FAQs

A thermostat is the brain of an HVAC system. It communicates with the furnace, air conditioner, or heat pump, telling the system when to turn on and when the desired temperature has been reached. The thermostat has temperature sensors that enable it to know your home’s temperature. 

Today’s newer units are digital thermostats and can automatically switch between heating and cooling based on the indoor temperature.

If you see the word Hold on your programmable thermostat, it means you can press a button or the touchscreen to hold the temperature at a certain level. This can be helpful if you have guests who need a warmer temperature than your normal schedule would provide, for example.

You can set it to Hold the temperature for a specific amount of time, and then depending on the model, the thermostat will return to its normal schedule. Sometimes you have to remember to turn off the Hold. Hold is not the same as Vacation Mode, which generally means you want to set the temperature much lower or higher than you would want it if you were home.

The best home thermostat is one that is compatible with your HVAC system and one that has features you will use. If you’re not very tech-savvy, you might not use all of the features of a smart thermostat, but the remote diagnostics feature of smart thermostats may be appealing to you.

Whether you’re considering thermostat replacement because your old thermostat doesn’t work anymore or you’re getting a new HVAC system and are trying to decide between Trane thermostats, talk with your local Trane dealer about your best options.

Your thermostat replacement cost will vary depending on the model you choose. Your final cost will include the product cost and the cost of thermostat installation. This cost is included in the cost of more comprehensive services such as HVAC replacement or installation. For optimal results, you should have an HVAC professional install and set up your programmable thermostat or smart thermostat.

If your Trane thermostat is not working, check out the following for help.

If you are still having problems, contact your local Trane dealer for assistance.

Read more about smart thermostats for homes

Contact a local dealer

Dealers can answer questions, help you find the right products for your home, and repair your system.

We’re here to help

Connect with our Customer Care team about your products, warranties, and dealer concerns.

Available Monday – Friday from 7am to 5pm CST

1-833-298-3493

A phone

brand pixel
What do you need help with?