HVAC Dealer in Seaford, Delaware
National HVAC Service
Company Details:
Seaford, Delaware
National HVAC Services
The National HVAC Service was originally founded in 1991 and was designed to provide a number of services, such as heating and air conditioning. It has served customers from multiple market sectors, such as the commercial, industrial and institutional market areas. This HVAC services company is privately owned and is a member of the Service Logic division. Its headquarters are located in Wexford, Pennsylvania.
Service Area
While the company started in Pennsylvania, the range of this company has expanded markedly. Now, the company operates all over the United States, including Arkansas, Massachusetts, Delaware and Tennessee. All of these locations work together via shared systems, programs, resources and cross-coverage and support from the Service Logic parent company. This range has allowed it to expand its customer base and compete with some of the leading names in the HVAC industry, such as Trane.
Services Provided
The National HVAC Service provides numerous services to its customers. Examples include long-term, guaranteed maintenance agreements and system installations. The company regularly comes out to test the various components of its systems to detect problems before they arise. Technicians come out to clean, lubricate, and adjust various maintenance components to keep them functioning at a high level, and if any of the components appear broken or worn down, they can be repaired or replaced on the spot. Should anything break, the company also provides an emergency repair system that functions 24 hours a day. The National HVAC Service's dedication to its customers has made it a leading name in the industry.