Cotes Mechanical is proud to serve the Sanger, Texas area with installation and service of both residential and commercial heating and air conditioning systems. For over ten years Cotes Mechanical has provided installation of new Trane heating and air systems as well as routine maintenance and emergency repairs.
Customers are provided with high efficiency and energy-saving heating and air units as well as insulation installation and attic ventilation. There is a range of options available to choose from including oil, gas and electric furnaces, heat pumps and boilers. The Texas heat requires a high-efficiency central air conditioning system to keep the entire home or commercial building comfortable and cool. Routine maintenance on the unit and small repairs can save money on energy costs. For systems over ten years old a completely new system is often the more cost-effective option. Energy star rated Trane systems can help cut energy costs in both residential and commercial properties.
During cooler weather, an efficient heating system is needed to keep everyone warm. Our professional and trained Trane technicians can run a home energy audit to determine the efficiency of the heating system. This will reveal any weaknesses and problem areas that need to be addressed to keep the heating system at peak performance.
Air duct cleaning is another service offered by Cotes Mechanical to the Sanger, TX area. The heating and air conditioning system can pull dust and dirt into the vents which in turn leads to a build of debris in the ducts. Cote’s Mechanical has a highly successful air duct cleaning system which brushes and vacuums the debris out of the ducts to help keep homes and commercial buildings cleaner.
SANGER, Texas 76266
Need help? Answer a few questions to connect with a dealer who can help you find your best HVAC solution.
Please enter your zip code
Please take a short survey on what
you think about trane.com
The dealer you selected doesn't service your Zip/Postal code.
You can close and confirm your location on the form or view all dealers in your area.
We recommend using the latest version of Google Chrome, Microsoft Edge, or Safari