Join us for the
Trane Commercial Seminars - Puerto Rico
What is Energy Decarbonization?
- The energy we utilize in our facilities has different emissions factors.
- Decarbonization is a social, community and business imperative to reduce or offset the emissions required to run operations.
- Decarbonization commitments, efforts and milestones resonate with ESG investors and public domain stakeholders.
Energy Saving Strategies
This presentation will explore solutions for energy optimization on existing buildings, based on control system with focus on air distribution, cooling plant, cooling tower optimization and energy recovery for ventilation air flow considering energy and economic impact.”
Why Are Refrigerants Transitioning?
After viewing the presentation, attendees will be able to:
- Summarize the drivers behind the new regulations and legislation for HVAC refrigerants.
- Discuss the actions being taken both globally (via the Kigali Amendment to the Montreal Protocol) and domestically (via the U.S. EPA and Climate Alliance States).
- Discuss the science behind why and how HVAC refrigerants are evolving.
- Compare environmental impact, efficiency and safety of current and
next-generation refrigerant options.
What is a Linear Expansion Valve Kit and how does it work?
VRF technology is one of the fastest growing spaces in the HVAC industry. It is an efficient solution that can also help buildings reach decarbonization and sustainability goals. Traditionally VRF systems are limited in their type and size of indoor equipment. Through the use of LEV/Air Handler Expansion kits, air handler options can be expanded and provide engineers more flexibility to meet a building’s specific load, air flow, and application requirements.
Meet our Speakers
Daniel Gentry
Applications Engineer
Trane Commercial North America
Dan Gentry is an Applications Engineer based in La Crosse, WI. He joined Trane in 2018 after 8 years at another local WI based chiller manufacturer. Dan first interned at Trane in the Technology Lab while attending school through 2008. His areas of expertise revolve around chiller plants, heat recovery and heat pump systems and their reliable and efficient design and operation.
He graduated from Ferris State University in 2011 with a bachelor’s degree in HVAC Engineering Technology and is an active member of ASHRAE.
Dan enjoys spending time with his family on the river and relaxing time at the family cabin up north.
Fernando Campos
LAR Energy Engineer
Trane Commercial, LATAM
Graduated from the Higher School of Mechanical and Electrical Engineering of the National Polytechnic Institute as a Mechanical Engineer with a Specialty in Thermal and Hydraulic Machines, master's degree in energy management and renewable resources at the Instituto Tecnológico de Monterrey Campus Estado de México.
Working at Trane since 2012 with participation in energy analysis and economic feasibility of energy improvement projects in new and existing projects, currently developing the position as Latin America Region Energy Engineer.
Joe Cefaly
Sr. Manager, Hydronics System Engineer – CEM, LEED AP
Mitsubishi Electric Trane HVAC US LLC
Joe Cefaly is currently Sr. Manager, Hydronics System with Mitsubishi Electric Trane and has 17 years of experience in the HVAC industry.
Joe graduated from Union College in 2003 with a B.S. in Physics and from Northeastern University in 2011 with an MBA.
In his spare time, Joe enjoys dirt biking and other motor sports.