Trane Rental Solutions Ensure Comfortable Environment for Visitors During the IAA 2013 Motor Show in Germany

Brussels, Belgium, 09 October, 2013 – Messe Frankfurt GmBH is the world’s largest trade fair corporation with its own exhibition grounds. The company has recently selected Trane, a leading global provider of indoor comfort solutions and services and a brand of Ingersoll Rand, to fulfill their additional, temporary cooling needs during the 65th International Motor Show (IAA) in Frankfurt am Main, Germany.

IAA is the oldest and most comprehensive show of the automotive industry gathering car developers, manufacturers and enthusiasts from all over the world. To provide visitors with the right environment to comfortably enjoy the show, leaders at the Messe Frankfurt GmBH have asked Trane Rental Solutions to supply additional cooling capacity for their Exhibition Hall 3.

As a result, they decided to implement two air-cooled helical rotary RTAD180 chillers with the total cooling capacity of 1,5 MW for the time period between September 4th – 25th.

The Exhibition Hall 3 is one of the most attractive and modern exhibition halls in Europe, with two levels offering exhibition space of approximately 38,000 square meters. During the IAA, the hall hosts the displays of one of the leading European car manufacturers and is expected to attract thousands of visitors.

“Cooling is critical for most businesses, whether it is to create the right indoor environment for buildings during special events or to provide reliable cooling for industrial processes,” said Andreas Stach, rental service sales engineer at Trane Germany. “With Trane rental solutions being specifically re-engineered for rental applications and selected for fast installation and easy operation, we were able to provide the IAA with the right answer to address their needs quickly and effectively.”

The impressive glassed-in hall structure of Exhibition Hall 3 has been designed by the British star architect and industrial designer Nicholas Grimshaw. There are no supporting columns inside the upper level of the glass hall, which means there are almost no limits to the height and width of the displays that can be set up there. Visitors are brought to their desired destinations by a number of escalators and passenger lifts. Refreshments are offered in four bistros, two restaurants and a bar.

Supplemental and back-up solutions help meet non-permanent cooling requirements in a wide variety of facilities, including healthcare, industrial environments, hospitality and retail. Temporary cooling needs can arise due to emergencies, capacity planning, planned maintenance and outages as well as in case of special events or for special applications.

The Trane online portal enables customers to easily obtain information on chiller rental range and availability in different countries across Europe, the Middle East and India.

# # #

About Messe Frankfurt

Messe Frankfurt is one of the world's leading trade show organizers with 536.9 million euros in sales and 1,833 active employees worldwide. The Messe Frankfurt Group has a global network of 28 subsidiaries and approximately 50 international sales partners, giving it a presence for its customers in more than 150 countries.

Events “made by Messe Frankfurt” take place at more than 30 locations around the globe. In 2012, Messe Frankfurt organized 109 trade fairs, of which more than half took place outside Germany. Messe Frankfurt’s exhibition grounds, featuring 578,000 square metres, are currently home to ten exhibition halls and an adjacent Congress Center. The company is publicly owned, with the City of Frankfurt holding 60 percent and the State of Hesse 40 percent. For more information, please visit our website at:

About the IAA

The International Motor Show (IAA) is the world's most comprehensive show of the automotive industry for everybody who develops, manufactures or uses passenger cars. A special feature is the large presence of suppliers throughout the whole automotive value added chain. Over 300 exhibitors from the supply industry are presenting their products. The origins of the IAA can be traced back to more than 115 years. Due to its high visitor and exhibitor turnout, the IAA was developed into a yearly alternating exhibition of passenger cars and commercial vehicles in 1991.

The 65th International Motor Show 2013 is held in Frankfurt am Main, Germany from September 12-22, 2013.

Trane Celebrates 100 Years

Founded in 1913 by James Trane and his son Reuben, Trane has a long history of industry-defining innovations for heating, ventilation and air conditioning systems. It is a leading provider of indoor comfort solutions and services and a brand of Ingersoll Rand. Celebrating its centennial this year, Trane continues to develop innovations in high performance building technologies, operating practices and intelligent building services that will create better, healthier, more comfortable and more productive indoor environments in the years to come.

About Ingersoll Rand

Ingersoll Rand (NYSE:IR) advances the quality of life by creating and sustaining safe, comfortable and efficient environments. Our people and our family of brands—including Club Car®, Ingersoll Rand®, Schlage®, Thermo King® and Trane® —work together to enhance the quality and comfort of air in homes and buildings; transport and protect food and perishables; secure homes and commercial properties; and increase industrial productivity and efficiency. Trane solutions optimize indoor environments with a broad portfolio of energy efficient heating, ventilating and air conditioning systems, building and contracting services, parts support and advanced control. Ingersoll Rand is a $14 billion global business committed to a world of sustainable progress and enduring results. For more information, visit or

Contact Information

Anne Blommaert

+32 2 746 1864

Perri Richman