Trane Compact Vertical Blower Coil Capable of Improving Energy Efficiency by up to 66 Percent

Trane Compact Vertical Blower Coil Capable of Improving
Energy Efficiency by up to 66 Percent

Using advanced technology, the new blower coil reliably and efficiently
delivers the comfort building occupants expect

DAVIDSON, N.C., July 27, 2016 – Trane, a leading global provider of indoor comfort solutions and services and a brand of Ingersoll Rand, introduced the addition of a new compact vertical blower coil to the terminal products portfolio — a complete family of products that deliver improved efficiency, ease of installation, acoustics and temperature control.

Available as a single-zone variable air volume (VAV) system with Tracer™ UC400 controllers, the blower coil can deliver up to 66 percent higher efficiency, temperature stability, quiet operation and dehumidification advantages for varying-occupancy space, ensuring occupant comfort.

Trane Single Zone VAV systems combine electronically commutated motors (ECM) and factory programmed variable speed controllers that adjust the speed of the unit’s motor and its air volume to meet unique load requirements in various spaces of a building. Because it precisely matches load requirements, the motor’s variable speed technology is ideal in partial load conditions.

 “For applications, like schools, where available space is a concern, the new Trane® compact vertical blower coil is a low profile air solution able to fit in small spaces that can be easily relocated, as building needs change,” said Eve London, terminal products manager for Trane Service. “The blower coil is designed with the service panels located in the front of the unit to provide customers with an easy installation, startup and services process.” added London.

Additional flexible design and configuration options include simple or complex controls, coil options and piping packages, making it an affordable system solution for a variety of building applications.

Terminal products also feature soft ramp technology that slowly increases and decreases fan speeds, adjusting to maintain temperature settings while dehumidifying the air. This improves indoor air quality by reducing the potential for mold or harmful bacteria in the building. Soft ramp technology also improves system acoustics by providing minimum air volume and eliminating noisy on and off cycling.

To learn more about Trane terminal technology products, visit

# # #

About Ingersoll Rand and Trane
Ingersoll Rand (NYSE:IR) advances the quality of life by creating comfortable, sustainable and efficient environments. Our people and our family of brands — including Club Car ® , Ingersoll Rand®, Thermo King ® and Trane ® — work together to enhance the quality and comfort of air in homes and buildings; transport and protect food and perishables; and increase industrial productivity and efficiency. We are a $13 billion global business committed to a world of sustainable progress and enduring results. Trane solutions optimize indoor environments with a broad portfolio of energy efficient heating, ventilating and air conditioning systems, building and contracting services, parts support and advanced control. For more information, visit  or .


Contact Information

Heidi McGuire


Minda Kuckuck