Virginia DMV Wins Trane Energy Efficiency Leader Award

FOR IMMEDIATE RELEASE

Virginia DMV Wins Trane Energy Efficiency Leader Award

Virginia DMV Leaders Expect Upgrades to
Reduce Energy Consumption by 36 Percent

Gov. McAuliffe Announces Executive Order at Award Ceremony

Richmond, Va., Nov. 5, 2014 - Leaders at the Virginia Department of Motor Vehicles (DMV) expect recently completed upgrades to the state DMV building located in Richmond, Virginia, to reduce energy consumption by 36 percent and save $284,000 a year.

The majority of the upgrades to the 310,650 square-foot, nine-story facility were completed to address aging and outdated infrastructure. The project supports Gov. Terry McAuliffe’s recently released Energy Plan and his new Executive Order on reducing energy consumption in state buildings.

The building upgrades also are helping to improve the comfort of DMV visitors and employees while reducing the state’s environmental impact. The improvements address building infrastructure systems approaching the end of their useful life.

In recognition of the Virginia DMV’s commitment to energy and operational efficiency and sustainability, Trane, a leading global provider of indoor comfort solutions and services and a brand of Ingersoll Rand, recently presented DMV with the “Energy Efficiency Leader Award” which recognizes the agency as a national leader in reducing its environmental impact,

“These improvements address building systems that were at the end of their useful life while providing significant cost reductions for the state,” said Richard D. Holcomb, Virginia DMV Commissioner. “The upgrades enable DMV to exceed state requirements for energy efficiency while creating a more comfortable and productive environment for customers and employees. The upgrades so significantly reduced our energy costs that our utility company actually called us to see if we had shut down a third of our building!”

DMV funded most of the improvements with a performance contract, made possible through a program managed by the Virginia Department of Mines, Minerals and Energy.  DMV also worked closely with the Department of General Services and the Department of the Treasury for the effort. The performance contract allowed DMV to use future energy and operational savings to help finance the infrastructure improvements up front. Performance contracting is a funding option that provides measurable business results to support strategic business objectives.

Prior to completing the upgrades, DMV conducted a detailed energy audit of the building which identified a list of potential energy conservation measures. Building information modeling was then used to evaluate potential solutions and their benefits. DMV then selected the solutions that best met its needs based on energy savings and other factors.

Upgrades to the DMV building included replacing all interior and exterior lighting systems with highly efficient illumination. Water retrofits were completed throughout the building to increase energy efficiency and conserve water. Chilled water system upgrades included installing two new centrifugal chillers, variable flow drives and deduct meters which help reduce sewer fees for cooling tower water.

The project team replaced outdated pneumatic building controls to allow for chiller plant optimization and control of the heating plant, lighting system and other solutions throughout the building. The team also replace 500 Internal Server Error

Internal Server Error

Cannot serve request to /content/trane-commercial/north-america/us/en/about-us/newsroom/press-releases/-virginia-dmv-wins-trane-energy-efficiency-leader-award.html on this server


ApacheSling/2.4 (jetty/9.2.9.v20150224, Java HotSpot(TM) 64-Bit Server VM 1.8.0_131, Linux 4.14.33-51.37.amzn1.x86_64 amd64)