This is the login for Trane® Connect™ and other Trane® commercial applications. Trane® Connect™ is our secure, cloud-based customer portal to access your building systems to remotely monitor and manage building systems, and conduct routine maintenance.
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
Customer Story & Case Study

Hospital Cite de la Sante Laval

Hopital Cité de la Santé, Laval, installed a Trane system, reducing energy costs and emissions. The system ensures optimal performance and comfort, supporting LEED certification.

Quick Facts

Industry
Healthcare
Products
Waterside, Chillers, Boilers • Geothermal Systems • Series R Helical Rotary Screw Chillers • Tracer Summit • Building Automation Systems
Topics
Optimal Comfort • Energy Efficiency • Cost-Saving • Sustainability
Services
HVAC Services

The Challenge

As the Hopital Cité de la Santé, Laval, made plans for an extension to its existing hospital building, facility managers outlined their criteria for a new HVAC system. To reduce energy consumption and carbon emissions, a geothermal system was specified. The hospital also required a boiler, for redundancy and back up, due to the critical nature of the facility’s operation.

The Solution

Having good knowledge of geothermal systems, but without similar installation in their other facilities, it was critical for the hospital to select a knowledgeable systems supplier. The job was bid to established manufacturers with geothermal experience. Based on the best product performance with the geothermal application, the company’s reputation for service excellence and a previous successful relationship, Trane was
selected as the hospital’s project supplier. Trane worked with the engineers to select a system that would provide the cold evaporator temperatures required for the application.

Central geothermal system offers energy efficiency

Geothermal systems use the earth’s renewable thermal energy for heating and cooling. These systems can generate significant operating cost savings and reduce carbon emissions. The Trane central geothermal system, designed for the hospital, combines the energy efficiency of geothermal with the benefits of a centralized heating, cooling and air handling system to provide an even more efficient and comfortable solution than traditional geothermal systems.

The Trane central geothermal system consists of two chillers coupled with a closed, ground geothermal loop which exchanges heat with the earth. The system offers high energy efficiency, and with all major equipment centrally located in the mechanical room, provides the additional benefit of centralized service and maintenance. In addition, the quiet operation of the system helps to ensure a restful environment for patients and staff.

Chillers provide high-performance and heat recovery

After reviewing a variety of options, two Trane lowtemperature Series R™ Helical Rotary Water-Cooled Chillers (RTWD), with water-to-water heat pump controls and heat recovery capability, were installed. The proven reliability and flexible design of the Trane rotary chiller makes it a perfect match for high-performance applications, such as the hospital’s geothermal system.

With fewer moving parts and a low-speed/direct drive compressor, the advanced helical rotary chiller improves energy efficiency and requires less maintenance. The chiller also provides consistent performance to enable the hospital’s mission critical operations.

The RTWD is engineered to maintain tight tolerances for precise temperature control. The chillers can be configured to produce leaving-evaporator solution temperatures as low as 10°F (-12°C), making it ideal for the geothermal application. The RTWD is also well suited for energy-saving heat recovery.

Control application enables optimal system performance

A Trane® Tracer Summit™ building automation system (BAS) provides integrated control, allowing the building operator to perform daily tasks, such as responding to alarms, viewing reports and trends, and custom programming. Facility managers use the Chiller Plant Control application to commission an extensive sequence of operations to achieve the highest level of system performance and ensure optimal energy management. Trane-provided training on the operation and programming of the BAS enables operators to take advantage of their control system’s full capabilities.

Service keeps systems running at their best

The geothermal chillers include a five-year parts and labor warranty, and a service contract. Under the agreement, factory authorized technicians perform periodic maintenance needed to keep the systems running at their best, eliminating unplanned downtime for the critical hospital operations and helping to avoid costly emergency service calls.

The Results

The Trane central geothermal system installed for the extension of the Hopital Cité de la Santé, Laval, is keeping patients, staff and visitors comfortable, while helping the CSSS Laval achieve its energy performance and sustainability objectives. The system has lowered energy costs and reduced greenhouse gas emissions, achieving points for LEED certification. The efficient geothermal system has operated without failure, making use of the hospital’s backup system unnecessary, even at temperatures as low as -28°C (-18°F) in the Montreal Region.

Customer Stories

Learn how we’ve helped other customers.

    • Customer Story & Case Study

    Campbellford Memorial Hospital and Trane

  • Asante_Rogue_Regional_Medical_Center_535x339.jpg
    • Energy Efficiency
    • Customer Story & Case Study

    Asante Rogue Regional Medical Center

    Asante Rogue Regional Medical Center added a fifth chiller and updated controls with Trane, saving nearly $187,000 annually and increasing redundancy and energy efficiency.

  • Senior patient and nurse in hospital
    • Indoor Environmental Quality
    • Customer Story & Case Study

    Jewish Eldercare Centre

    Jewish Eldercare Centre upgraded its HVAC with Trane's geo-exchange system, saving $250,000 annually and improving comfort and reliability for residents.

Help is closer than you think.

Work with dedicated local Trane representatives who can team with you to solve your problems while providing training and insights.

Find Your Trane Rep Contact Us
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
Privacy Policy English | French 
Terms of Use English | French

All trademarks referenced are the trademarks of their respective owners.

© 2026 Trane. All Rights Reserved.

Trane Technologies