Trane Introduces Technologies to Further Optimize Comfort and Energy Efficiency
New options offered by the Performance Climate Changer™ Air Handler address building environment and performance
Chicago, IL May 5, 2010 - It is no longer enough for heating, ventilation and air conditioning (HVAC) systems to simply deliver "conditioned air." That is why today Trane is introducing its Performance Climate Changer™ air handler with cataloged capacities up to 60,000 cfm. The Performance air handler features energy recovery, airflow monitoring, and advanced humidity control options that improve the building environment and better control temperature and humidity, while optimizing performance.
These options include Trane Cool Dry Quiet (CDQ™) desiccant dehumidification wheels, energy recovery wheels, direct-drive plenum fan arrays, and dual-path split dehumidification units. When combined with the existing benefits of low pressure drop, enhanced filtration and optimized casing designed for minimal leakage, the Performance air handler provides unmatched filtration, option flexibility and airflow efficiency. These latest technology advances enable a Performance Climate Changer HVAC system to deliver optimized performance with up to 30 percent fan energy savings compared with the previous generation air-handling units.
"As we become an increasingly global society, the importance of energy and operational efficiency cannot be minimized," said Gina Cottrell, global airside business leader at Trane. "The innovations of the Performance Climate Changer air handler provide superior performance for commercial, institutional and industrial buildings worldwide as well as increase the comfort and productivity of the people in those buildings."
Systems utilizing the Performance air handler deliver optimized HVAC performance with measurable energy savings. This air handler can be applied with chilled water systems and control systems in a low-flow, low temperature HVAC system designed to reduce energy consumption by up to 30 percent, while helping to reduce emissions, lower first cost and operating cost, and provide better comfort with lower space humidity.
Product Photos
![]() |
![]() |
![]() |
|---|---|---|
| The Performance Climate Changer™ air handler (Cut-away View.JPG) | The Performance Climate Changer™ air handler (Split View .JPG) | The Performance Climate Changer™ air handler (Whole View .JPG) |
About Trane
Trane, a business of Ingersoll Rand - the world leader in creating and sustaining safe, comfortable and energy efficient environments - improves the performance of homes and buildings around the world. Trane solutions optimize indoor environments with a broad portfolio of energy efficient heating, ventilating and air conditioning systems, building and contracting services, parts support and advanced controls for homes and commercial buildings.
For more information, visit www.Trane.com