TRANE FOR ENGINEERS
TRANE FOR ARCHITECTS
TRANE FOR DATA CENTERS
TRANE FOR HEALTHCARE
 

Case Study - Higher Education

Donald Bren Hall

Download PDF | Print
Flash 8 is required to view this component.
Get Adobe™ Flash Player Get Adobe™ Flash Player

AT BREN HALL, SUSTAINABLE CONSTRUCTION, ENERGY MANAGEMENT AND SOUND ENVIRONMENTAL PRACTICES ARE FACTS OF LIFE

University Building Achieves LEED™ Platinum Rating for Environmental Design

A Living Laboratory for Training Environmental Management Professionals.

The Donald Bren School of Environmental Science & Management was created to help fill California’s need for trained environmental professionals, and what better way to educate them than to put them into a living example. The school’s advisory board recommended that the building, as a top environmental school, should exemplify the school’s goals. As a result, Bren Hall was built using the USGBC LEED guidelines, with the goal of exceeding the California Energy Code’s Title 24 standards for energy efficiency. In fact, the building includes so many environmentally sound elements, it achieved a Platinum rating, the highest available under the U.S. Green Building Council’s (USGBC) Leadership in Energy and Environmental Design (LEED)™ program.

EarthWise™ Efficiency for an Innovative Chiller Loop.

It’s no surprise that the chiller selected for Bren Hall was an EarthWise CenTraVac™ from Trane. The high efficiency 350-=ton chiller, which uses r-123, a more environmentally friendly refrigerant, is now part of the chilled water loop that serves the entire University of California at Santa Barbara campus. This innovative loop design allows the building with the most efficient chiller for a given system load to be used to meet the cooling demand of any other building on the loop. The Bren Hall chiller plant also utilizes a TRANE Tracer Summit™ chiller plant control system to enable continuous energy use monitoring. This allows operators to analyze and optimize system efficiency to minimize demands on resources.

In addition to efficient cooling, Bren Hall features a wide variety of innovative green architectural elements that help with energy management. They include a white-cap roof to reduce heat gain; natural ventilation design that takes advantage of Pacific breezes, and an advanced lighting plan that uses as much daylight as possible and monitors lighting based on actual room usage.

A Green Laboratory Building for a Green Curriculum.

Bren Hall has achieved a remarkably low annual energy use rate of only 1.1 kWh per square foot, which exceeds the California Energy Code requirements by 31 percent. CenTraVac’s extremely low refrigerant leak rate—no refrigerant has been added to any of the total of 3,800 tons of Trane chiller capacity on the campus in the past six years—means no environmental impact due to refrigerant emissions. Trane’s high efficiency chillers also lower energy demands, reducing electric power plant emissions. All of which contributes to Bren Hall’s status as an award-winning green building with the distinctive Platinum LEED certification. Trane’s CenTraVac is the environmentally smart chiller for an environmentally advanced campus. Talk to us; we’ll help you create High Performance Buildings for Life.

THE SPECIFICS

Expand

Close

THE SPECIFICS

BUILDING TYPE

Classrooms, research laboratories and offices.
Square Footage
84,672 sq. ft.

PROJECT TEAM

  • University of California FacilitiesManagement Group
  • Zimmer, Gunsul, Frasca architects
  • Trane

SYSTEMS INSTALLED

  • TRANE Model CVHE centrifugal chiller
  • TRANE Tracer Summit™ automation system
  • Variable frequency drives on chilled water, condenser and cooling tower pumps
  • Variable speed air handler and terminal box fans to optimize air supply and energy use

About the Donald Bren School of Environmental Science & Management

UCSB, on the Pacific Coast north of the city, has nearly 20,000 students and a faculty of 1000. UCSB has a wide academic offering, including the Bren School which opened in 1994. The School is housed in Bren Hall which opened in 2002 and includes classrooms, research laboratories and offices. The building’s sawtooth design allows maximum view and natural light. Offices use natural, flow-through transom ventilation. Many areas are shaded with a two-story, vine-covered trellis. Many materials are of environmentally compatible and recycled materials, including concrete, wallboard, carpeting, partitions, countertops and furniture. Flooring and paneling are 100 percent recycled/recyclable materials.