U.S. Consumer Product Safety Commission – Recall Alert   

Recall Date: August 14, 2015


Trane and American Standard Recall Accessory Heaters Due to Fire Hazard (Recall Alert)


Recall Summary

Name of Product: Accessory heaters installed in TAM7 and TAM8 air handlers

Hazard: Heaters installed with reverse polarity on one of the breakers can cause the heater to overheat, posing a fire hazard.

Remedy: Replace

Consumers should immediately stop using the heater function by switching the system to cooling mode or off and contact their Trane or American Standard independent dealer to schedule an inspection and replacement. The system’s air conditioning or cooling function may still be used. Trane is contacting its customers directly.

Consumer Contact: Trane toll-free at 844-866-8429 from 8 a.m. to 5 p.m. CT Monday through Friday, or online at www.trane.com/residential orwww.americanstandardair.com and click on “Safety Recall” for more information.

Recall Details

Units: About 3,900

Description: This recall involves Trane and American Standard brand accessory heaters manufactured between November 2014 and March 2015 and installed in TAM7 and TAM8 air handlers as a primary or secondary heat source. Models included in the recall are BAYEVBC15BK1BAA (15 KW Electric Heater) with serial numbers 1447B2BP1X through 1512B2CDDX and Model BAYEVCC25BK1BAA (25 KW Electric Heater) with serial numbers 1503B2AP0X through 1513B2BHXX. Due to the electrical risk, only a certified HVAC repair person should verify the model and serial numbers on the nameplate on the inside of the air handler.

Incidents/Injuries: The firm has received 10 reports of the heaters tripping circuit breakers, including one report of heat-related damage to the unit. No injuries have been reported.

Sold at: Trane and American Standard independent dealers nationwide from January 2015 to April 2015 for about $120.

Importer: Trane U.S. Inc., of Tyler, Texas

Manufactured in: Mexico


Photo 1: BAYEVBC15BK1BAA (15KW)

Photo 2: BAYEVCC25BK1BAA (25 KW)

About U.S. CPSC: The U.S. Consumer Product Safety Commission is charged with protecting the public fromunreasonable risks of injury or death associated with the use of thousands of types of consumer products under the agency’s jurisdiction. Deaths, injuries, and property damage from consumer product incidents cost the nation more than $1 trillion annually. CPSC is committed to protecting consumers and families from products that pose a fire, electrical, chemical or mechanical hazard. CPSC’s work to ensure the safety of consumer products - such as toys, cribs, power tools, cigarette lighters and household chemicals – contributed to a decline in the rate of deaths and injuries associated with consumer products over the past 40 years.

Federal law bars any person from selling products subject to a publicly-announced voluntary recall by a manufacturer or a mandatory recall ordered by the Commission.

To report a dangerous product or a product-related injury go online to www.SaferProducts.gov or call CPSC’s Hotline at (800) 638-2772 or teletypewriter at (301) 595-7054 for the hearing impaired. Consumers can obtain news release and recall information at www.cpsc.gov, on Twitter @USCPSC or by subscribing to CPSC’s free e-mail newsletters.

CPSC Consumer Information Hotline

Contact us at this toll-free number if you have questions about a recall:

800-638-2772 (TTY 301-595-7054)

Times: 8 a.m. – 5:30 p.m. ET; Messages can be left anytime

Call to get product safety and other agency information and to report unsafe products.

Media Contact

Please use the phone numbers below for all media requests.

Phone: (301) 504-7908

Spanish: (301) 504-7800