Commercial Real Estate


Commercial Facilities Services

The outside and common areas of the two Corporate Plaza office buildings, managed by Commercial Facilities Services, had been recently remodeled and mechanical systems had been replaced. With utility costs continuing to run high, the property manager sought to further improve the facilities’ energy efficiency. As the company looked for solutions, they zeroed in on the buildings’ aging controls systems.

Read More

Von Braun Center

Originally built in 1974, the Von Braun Center has doubled in size over the years with four major expansions, and plans underway for construction of another 150,000 sq ft of space. While the renovations have allowed the center to increase the activities it can over, the additions have also contributed unfavorably to the performance of the facility’s mechanical systems.

Read More

Bank of America Stadium

Faced with the need for additional cooling capacity, high energy costs, and an aging infrastructure, Bank of America Stadium, home of the Carolina Panthers, was also challenged by a short off-season. With events already scheduled and tickets sold, it was critical that needed upgrades adhere to strict deadlines in order to provide comfort for stadium guests, and alleviate the inconvenience and financial burden of cancellations.

Read More

Lincoln Square South

Centralized chiller plant improves energy efficiency and occupant comfort; operates at .49kW/ton in part-load conditions.

Read More

California State Lottery Headquarters

Solar plus storage create Zero Net Energy pavilion; reduce utility costs; help achieve LEED Gold® certification

Read More

Filter

Top