Trane Launches New Sintesis™ Advantage CXAF HEat Air-to-Water Heat Pumps
Sintesis™ Advantage CXAF HEat Improves full load and seasonal efficiency in heating mode with no impact on footprint
Trane®, a leading global provider of indoor comfort solutions and services and a brand of Ingersoll Rand, introduces a new air-to-water heat pump CXAF HEat (High Efficiency) model to its proven Sintesis™ platform of high efficiency large air-cooled chillers.
With heating capacity between 270 to 700 kilowatts (kW), the new
CXAF HEat unit features an advanced suction line gas heat exchanger
that boosts heating capacity with no significant increase in energy
consumption compared to the SE (Standard Efficiency). At the same time
it delivers improved full load and seasonal efficiency in heating mode
within the same spatial footprint and sound level.
The CXAF can operate down to negative 15 degrees Celsius producing hot water of 45 degrees Celsius without the need for auxiliary heating, making it suitable for most European climates and a more reliable and efficient alternative for gas or fuel boilers.
“The Sintesis CXAF portfolio is the result of our belief in electrification of heating as a way to offset the use of fossil fuels for heating and an important global contributor to mitigate climate change and reduce carbon footprint.” said Sai Srikanth Pinisetti, engineering leader for Trane Europe. “By adding the new CXAF HEat to our portfolio we continue offering our customers options for sustainability and better efficiency thus contributing to our vision of reducing the energy intensity of the world.”
Trane CXAF customers can benefit from:
- Cooling or heating from one single package - the reversible technology lowers installation and operating costs by satisfying summer and winter demands with a single unit.
- Operating ranges down to negative 15 degrees Celsius in heating mode, and up to 52 degrees Celsius in cooling mode making it suited for comfort and industrial applications.
- Wide range of configurations to choose from, combining low noise and high efficiency to minimize the Total Cost of Ownership.
- Choice of three levels of noise attenuation to meet the requirements of even the most sound-sensitive environments.
- Full interoperability via SmartCom interface LonTalk®, BACnet® and Modbus.
The units offer best in class, Eurovent Class A efficiency in
heating and seasonal efficiency exceeding minimum regulatory
requirements. All units in the Trane Sintesis Advantage portfolio are
compliant with all applicable European Ecodesign Regulations under the
Energy-related Products (ErP) framework Directive 2009/125/EC of the
European Parliament.
For more details of on the complete Trane portfolio of solutions, please visit Trane.eu.
# # #
About Ingersoll Rand
Ingersoll Rand (NYSE:IR) is a world leader in creating and sustaining safe, comfortable and efficient environments in commercial, residential and industrial markets. Our people and our family of brands — including Club Car®, Ingersoll Rand®, Thermo King® and Trane® — work together to enhance the quality and comfort of air in homes and buildings, transport and protect food and perishables, secure homes and commercial properties, and increase industrial productivity and efficiency. Trane solutions optimize indoor environments with a broad portfolio of energy efficient heating, ventilating and air conditioning systems, building and contracting services, parts support and advanced control. Ingersoll Rand is a global business committed to sustainable business practices within our company and for our customers. For more information, visit www.ingersollrand.com or www.trane.eu.