Rental Capabilities

Trane Rental Services has an impressive array of HVAC, power generation and compressed air equipment. We can provide a single unit or a combination of units and build a solution to fit your needs. Our capabilities include 1-1,000-ton units of cooling, 36-1,500 kW of power generation, electric and indirect fired heaters up to 512,000 Btus, and 800 to 1,500 cfm Oil-Free Air units.

Contact Trane Rental Services at 800.755.5115

 

Literature

  • Rental Equipment Line Card
  • General Capabilities Brochure
  • General Product Catalog
  • Generator Product Catalog
  • Contingency Planning
  • Special Events
  • Education
  • Healthcare
  • Portable Moisture Removal
  • Oil-Free Compressed Air
  • Solutions for Wineries
  • Solutions for Warehouses
  • Solutions for Data Centers
  • Solutions for Ice Rinks
  • Solutions for the Tire Industry
  • Solutions for the Automotive Industry

What Every Event Needs

Your events come in all shapes and sizes, but they generally have one thing in common--– they are held in areas where power and temperature control are not easily obtainable.

Trane Rental Services has the right equipment to provide a temporary environment that ensures comfortable and successful events. With many years of experience in creating temporary environments, Trane Rental Services provides
you with the right equipment supported by OEM-trained engineers and technicians.

Benefits of using Trane temporary equipment.

We have one of the newest fleets in the industry to ensure reliable and aesthetically pleasing products.

Rental specific modifications that make equipment easier to install with quicker connections for power, water and duct work.

Our products are engineered to create comfortable, environmentally friendly events regardless of size, shape or geographic location.

We specialize in delivering reliable solutions in the most complex job situations.

View our capabilities for your Special Event.

Trane Rental Services has an impressive array of HVAC, power generation and compressed air equipment. We can provide a single unit or a combination of units and build a solution to fit your needs. Our capabilities include 1-1,000-ton units of cooling, 36-1,500 kW of power generation, electric and indirect fired heaters up to 512,000 Btus, and 800 to 1,500 cfm Oil-Free Air units.

 

Education

Schools and colleges have many unique temporary HVAC and power needs. Repairs and upgrades cannot always be scheduled during times when classes are out of session, but Trane Rental Services can keep classrooms unaffected during scheduled maintenance. Trane Rental Services can keep students and faculty focused on schoolwork rather than the temperature of the building. School administrators can rent chillers or other temporary cooling components to be installed quickly and easily to keep systems running while repairs or up- grades are made. 

Healthcare

Trane Rental Services provides an array of healthcare building temporary power and cooling solutions. Power and HVAC systems are crucial for the health of patients. If heating or cooling systems fail or if they need to be shut down temporarily, the results could be disastrous.

Many healthcare facility managers put a contingency plan into place as part of their emergency preparedness program. Trane’s rental emergency equipment often factors into these plans to help healthcare building HVAC administrators sustain patients’ comfort in the event of a catastrophe.

Industrial

Manufacturing and chemical operations often have unique industrial HVAC needs that Trane temporary rental chillers can help solve.

Manufacturers and laboratories sometimes need a temporary cooling system to back up critical manufacturing and chemical processes. In many cases, these businesses do not have redundancy or backup systems in place to minimize downtime. Usually these highly critical and sensitive processes could cause serious problems for the businesses or labs if the industrial HVAC system fails; so Trane’s temporary solutions are the perfect fit.

Trane offers standby equipment programs to provide peace of mind and minimize financial risks associated with downtime. Trane also has equipment that can be used during planned shut-down events or in during the seasons that require supplemental equipment.