ne

Questions & Answers









DEALER RELIABILITY

How is Trane CleanEffects™ different?

Trane CleanEffects™ delivers 8 times the amount of clean air as the typical room HEPA appliance, and 100 times the amount delivered by an ionic-type room appliance or a standard 1" filter — the kind found in 85% of homes.

The World’s Most Effective Air Filtration

Standard air cleaners on the market have filters that are very dense. Meaning, they try to stop the dust by trapping it in a slightly porous filter. The fewer the pores the more dust it can trap. However, this not only stops the dust and dirt, but it also stops the air from moving as well. This is called pressure drop.

The revolutionary Trane CleanEffects™ air filtration system has the lowest pressure drop with the highest efficiency possible. Our unique patented technology is designed to let air flow freely through the most advanced filtration system available. The result, more of your air is cleaned faster and more effectively than anything else on the market.

Trane CleanEffects™ utilizes patented air cleaning technology to remove up to 99.98% of airborne allergens from the air that passes through the filter, making it 8 times more effective than even the best HEPA room filters and up to 100 times more effective than a standard 1” filter. What’s more, Trane CleanEffects™ has been performance-tested by LMS Technologies and Environmental Health &Engineering, Inc. (EH&E), with the results verified by professors from the Harvard School of Public Health.

LMS Technologies is a technology consulting company that specializes in air flow measurement, filtration testing and particle analysis. Environmental Health & Engineering is an environmental consulting and engineering services company that is dedicated to ensuring safe and productive environments, and is co-founded by John D. Spengler, PhD of the Department of Environmental Health at Harvard.

Related Questions

  1. 1 What is Clean Air Delivery Rate?
  1. 2 How can I upgrade to CleanEffects™?
  1. 3 What are particulates?

Have more Questions? Talk to an Expert.

Trane - Comfort Specialist
Expanded links