ne

Questions & Answers









DEALER RELIABILITY

How can I make the air in my home cleaner?

The average American spends more than 90% of their time indoors, making them susceptible to unsafe particles and allergens. An efficient Trane system never stops working to ensure the air in your home is clean and breathable.

Reduce Allergens
As published in BioMed Central Journal, an independent publishing house committed to providing access to peer-reviewed biomedical research, Trane CleanEffects™ has been shown to reduce triggers for allergies and asthma. It removes up to 99.98% and particles and allergens from the filtered air. Installing Trane CleanEffects™ can be an important part of your overall allergy and asthma management plan.

Expert Allergy Tips
Here are allergy experts’ tips for managing allergies and asthma in the home:

  • Control dust mites — Use anti-dust mite covers and wash sheets in hot water at least once a week; 130 degrees is recommended.
  • Eliminate mold sources – Fix leaky pipes and keep bathroom grout clean.
  • Stay smoke-free — Avoid non-ventilated, smoky rooms and second-hand smoke.
  • Avoid pet dander — Keep pets off the furniture, out of the bedroom, and if necessary, consider taking the pet out of the home.
  • Close doors and windows — Keep windows and doors shut to keep outdoor pollens, molds and irritants outside.
  • Install a whole-house air cleaner — An air cleaning system, such as Trane CleanEffects™ removes airborne particles and allergens too tiny for your nose and mouth to filter naturally.

In addition to taking steps to control allergens in the home, you should always see an allergist to determine the cause of your symptoms. An allergy specialist can run a series of simple blood or skin tests to determine if your asthma symptoms are allergy-related.

Say Goodbye to Dust
Have you ever felt that no matter how often you dust the dust seems to reappear the next day? You’re not alone. The average six-room house collects 40 pounds of dust each year. New studies show that the installation of Trane CleanEffects™ reduces dust accumulation in your home by more than 50%.

Related Questions

  1. 1 What is Trane CleanEffects™?
  1. 2 How do I choose an air cleaner?
  1. 3 What are particulates?

Have more Questions? Talk to an Expert.

Trane - Comfort Specialist
Expanded links