Does Trane CleanEffects produce a harmful level of ozone?
No. Trane CleanEffects™ contributes a negligible amount of ozone – less than .3 ppb to the living space.
Trane CleanEffects™ was designed to fall well below the 50 parts per billion (ppb) FDA voluntary emission limit for medical devices, contributing less than .3 ppb of ozone to the living space. To put this into perspective further, typical ozone levels during the summer outdoors are at about 60 to 90 ppb, and indoor levels can vary greatly but are typically between 12 ppb to more than 80 ppb. Testing of Trane Clean Effects by third parties has shown there’s no more ozone in a home installed with Trane CleanEffects™ than naturally occurs in the environment already.