Reliability

At Trane, we don’t just build our products. We own patents on them. And we don’t just test our products. We push them to the extreme, because if it can’t make it through our torturous testing, you’ll never see it in your home.

BUILT BY TRANE

Every Trane product is designed down to every detail and rigorously tested for reliability and durability. While other manufacturers build their products from the same “pool” of parts available to anyone, we make it a point to be uniquely better, innovative and always looking to the future. To do that, we have to design, build, test, and rebuild some of our own parts. We know they work because we push them well beyond the industry standards, making sure they match the reliability people expect when they own a Trane. From the durable Climatuff® compressor to the exclusive Spine Fin™ coil to the revolutionary Hyperion™ air handler—and a number of other patented innovations—when you own a Trane, you’re getting more than reliable comfort and you’re getting it year after year.

TESTED TO EXTREMES

At the SEET lab in Tyler, Texas—which stands for Systems Extreme Environmental Test—Trane products are put through 16 weeks of bone-chilling cold and blistering heat, in repeating two-week sessions. Some units endure over 2,600 hours of continuous testing, including a full week of salt spray to monitor corrosion resistance. Our technicians have tried to break our Climatuff® compressor over 900 ways, which has produced a saying at Trane, if a product doesn’t make it through our test lab it doesn’t get made. By putting our heating and cooling units through 5 years worth of wear and tear in the matter of a few months, we reinforce our philosophy of making products you can rely on for years and years. It’s hard to stop a Trane isn’t just a tagline…it’s been proven.

BACKED BY EXPERTS

Every manufacturer will say that their products are the best, but when industry experts give a tip of the hat to your work, that’s backing it up with proof. Popular Mechanics dubbed the Trane ComfortLink™ II control as one of The Year’s Most Transformative Products, awarding it their 2010 Breakthrough Award. A Harvard-led, independent research project evaluated the air cleaning performance of several in-duct and portable devices, and found conclusively that Trane CleanEffects™ is the world’s most effective whole-house air filtration system. So, while we’re known for reliable heating and air conditioning, we also seem to be setting the industry standard in smart home and clean air technology, because your home comfort deserves constant innovation.

REAL-LIFE STORIES

Trane products are nearly unstoppable. Check out these real-life stories of Trane products that triumphed over the most extreme real-life situations imaginable.  See more.

NEED HELP? TALK TO AN EXPERT.
CONTACT YOUR LOCAL TRANE COMFORT SPECIALIST