Skip to page contents

Skip to Navigation

Home

Rebate Incentive Structure

This program runs through 2011. There are a limited amount of dollars for the rebate program so quick response is highly encouraged. Depending on the project, customers can expect to receive rebates as follows:

Program Year Incentive $/kW
Installation $1,400
2009 $200
2010 $200
2011 $200
Total $2,000

Shift now for a sustainable future

Let Trane and PG&E help you build a sustainable future as part of the $10M PG&E Shift & Save Program.

Trane U.S. Inc. has joined with Pacific Gas and Electric Company to help customers save money while shifting power demands to off-peak hours as part of the $10 million PG&E Shift & Save program. PG&E customers now have a sustainable, reliable, and environmentally friendly energy solution when the power grid is at risk of overload. By using state-of-the-art cooling technology, Trane will work with customers to install systems that will reduce peak demand by 1.2 MW, promoting grid reliability.

As part of a green initiative for California, Shift & Save uses Thermal Energy Storage (TES) to balance energy demands between daytime and nighttime and permanently remove daily AC peak loads over the entire cooling season. Using technologies that store energy in a thermal reservoir for later use, TES systems use ice or chilled water from stored thermal energy to reduce peak HVAC loads.

Download
Shift & Save flyer

For more information, please contact Trane's Shift & Save Customer Service Center at (866) 704-5161 and ask for John Burdette.

The Shift & Save Program is funded by California utility customers and is administered by PG&E under the auspices of the California Public Utilities Commission through a contract awarded to North California Trane. California customers who choose to participate in this program are not obligated to purchase any additional services offered by contractors. References to PG&E or its Shift & Save program do not constitute an endorsement or approval by PG&E or Trane.