Eligibility
The joint Trane/PG&E Shift & Save program provides for the installation of Thermal Energy Storage (TES) systems for the purposes of storing thermal cooling capacity during off-peak hours and/or partial-peak hours in order to meet thermal cooling load in subsequent on-peak hours. The Program's targeted customers are commercial, industrial, and agricultural customers as either a retrofit or new construction application in PG&E's electric service territory.
You are eligible to enroll in the program if you meet the following requirements:
- PG&E bundled customer
- Direct-purchase customer (must buy from PG&E directly, not an energy broker)
- Have a peak load shifting opportunity
- Have peak load dependent on outside air temperature
- Comfort cooling driven
Customers that will benefit the most from the Shift & Save program are those who are within one of these categories:
- Time of use utility rate structures (PG&E rates A6, A10, E19, E20)
- Healthcare
- K-12 and higher education
- Commercial office building
- Gaming and hospitality
- Retail
- Government institutions
Want more information? Contact Trane's Shift & Save Customer Service Center at (866) 704-5161 and ask for John Burdette, JBurdette@trane.com