Trane Expands Series of Cold Generator Scroll Chillers to Include Traditional and Compact Models

Trane Expands Series of Cold Generator Scroll Chillers to Include
Traditional and Compact Models

Scroll chiller portfolio is designed to meet comfort and process cooling needs
in a variety of new and existing facilities

Davidson N.C., July 30, 2015 — Trane, a leading global provider of indoor comfort solutions and services and a brand of Ingersoll Rand, has expanded the series of Cold Generator™ scroll water chillers to create a broad portfolio of optimized solutions to meet comfort and process cooling needs. Cold Generator scroll water chillers provide efficient performance and flexibility to serve a wide variety of new and existing facilities.

“This broad portfolio of scroll water chillers features traditional and compact models that include advance controls with Building Management System compatibility interfaces,” said Mike Filler, product manager for Trane. “Easy installation is critical in buildings with limited space or challenging room configurations, so each chiller is scaled for delivery through a standard doorway for ease of installation in new, retrofit, and renovation applications.”

Fit and flexibility of the units makes scroll water chillers ideal for new, retrofit and renovation applications in commercial and industrial applications, including historical buildings, education and healthcare.

The Cold Generator series includes the CGWQ and CCAQ series. The systems feature reliable scroll compressors with digital control technology that offer efficiencies at full- and part-load conditions. The scroll chillers also feature dual independent refrigerant circuits to reduce capacity loss in the event of a compressor failure.

In addition, the Cold Generator CGWQ and CCAQ series have a service friendly design allowing replacement of all major components without a complete unit teardown.

Cold Generator scroll water chillers are also available in compact models, including the CICA and CICB series. Each model has advanced controls and is able to function as a standalone chiller, or in an expandable array of up to 10 chillers similar to a single high capacity multi-stage package chiller. Cold Generator CICB compact water chiller is the newest addition to the compact series and has space-conscious design elements focused on convenience and serviceability.

Small or unusual room configuration can pose unique challenges for retrofit and renovation projects. With custom designed pipe sizes tailored to suit the specifications of unique spaces, the CICB compact scroll chiller can be installed in a variety of configurations, eliminating the cost and concern associated with replacing aging chiller equipment in a limited space.

Both the CICA and CICB compact series are AHRI-certified and compliant with ASHRAE 90.1-2013. Features of the CGWQ and CCAQ series include separate high-and low-voltage control panels, front access to all refrigerant components, brazed plate heat exchangers, and mechanically cleanable shell and tube condenser design for ease of maintenance and service.

Cooling systems play a critical role in the fundamental operation of buildings. The expanded portfolio of Trane Cold Generator scroll chillers provides tailored performance that helps meet comfort cooling needs and enhances the lives of building occupants.

To learn more about Cold Generator scroll water chillers, visit Trane.com/coldgenerator

# # #

About Ingersoll Rand and Trane
Ingersoll Rand (NYSE:IR) advances the quality of life by creating comfortable, sustainable and efficient environments. Our people and our family of brands — including Club Car ® , Ingersoll Rand ® , Thermo King ® and Trane ® — work together to enhance the quality and comfort of air in homes and buildings; transport and protect food and perishables; and increase industrial productivity and efficiency. We are a $13 billion global business committed to a world of sustainable progress and enduring results. Trane solutions optimize indoor environments with a broad portfolio of energy efficient heating, ventilation and air conditioning systems, building and contracting services, parts support and advanced control. For more information, visit ingersollrand.com or trane.com .