Trane Adds Water-Source VRF Systems to Growing Ductless Portfolio

FOR IMMEDIATE RELEASE

Trane Adds Water-Source VRF Systems to Growing Ductless Portfolio

Water-source VRF uses stable water temperatures to provide cost efficient heating and cooling solutions for multi-occupant buildings

Davidson, N.C., Nov. 6, 2014Trane, a leading global provider of indoor comfort solutions and services and a brand of Ingersoll Rand, has expanded its ductless portfolio to include the new Trane® Water-Source VRF Ductless Systems. The new systems provide energy-efficient climate solutions for multi-tenant and diversely occupied buildings, including commercial real estate, K-12 and higher education facilities.

Joining the Trane Air-Cooled VRF Ductless Systems, Trane water-source VRF uses water as the energy exchange medium to heat and cool the system’s condenser. Using adjacent water or geothermal sources, water-source VRF can draw upon stable water temperatures to dissipate heat during peak cooling periods and act as a heat source when in heating mode. Alternatively, systems can be connected to a cooling tower to reject energy from the building or a boiler to add heat in colder climate applications. Water-source VRF retains its heating capacity even as entering water temperatures fall because the drop is not as dramatic as it is with low ambient air temperatures. As a result, water-source VRF delivers up to 30.1 integrated energy efficiency ratio, 27.4 simultaneous cooling and heating efficiency and up to 48 tons of capacity.

“The growing portfolio of ductless products gives Trane one of the most comprehensive equipment, control and tool offerings in the industry,” said Jeff Peters, ductless portfolio leader at Trane. “Trane has the people and expertise to partner with contractors and engineers to help deliver intelligent solutions for every customer and any building.”

Water-source VRF allows building occupants to adjust the temperature in individual spaces for increased comfort. It also enables building managers to calculate the actual energy use of each leased space for more accurate tenant billing. Building managers have the flexibility to turn off airflow to unoccupied areas, which may result in significant energy savings.

Trane design experts can help specify VRF solutions for tall and historical structures, which often present unique challenges. Tall structures and buildings with large amounts of floor space require long piping runs and it is common for historical buildings to lack adequate ductwork. Water-source VRF uses small diameter piping instead of ductwork, helping to preserve the historical appearance of the building. The system can serve more than 984 feet of piping and has electronic expansion valves to efficiently heat and cool these spaces.

Trane plans to introduce additional ductless solutions in 2015. To learn more about water-source VRF and the growing Trane ductless portfolio, visit trane.com/VRF.

# # #

About Ingersoll Rand and Trane
Ingersoll Rand (NYSE:IR) advances the quality of life by creating comfortable, sustainable and efficient environments. Our people and our family of brands—including Club Car ® , Ingersoll Rand ® , Thermo King ® and Trane ® —work together to enhance the quality and comfort of air in homes and buildings; transport and protect food and perishables; and increase industrial productivity and efficiency. We are a $12 billion global business committed to a world of sustainable progress and enduring results. Trane solutions optimize indoor environments with a broad portfolio of energy efficient heating, ventilation and air conditioning systems, building and contracting services, parts support and advanced control. For more information, visit ingersollrand.com or trane.com .

Contact Information

Heidi McGuire

651-407-4000

heidi.mcguire@irco.com