Commercial :  Local sales offices :  About Trane

 


* Book Store  
* Building Services  
* Case Studies  
* Engineers Newsletter  
* Products  
* Market Segments  
* Financing  
* Global/Ntnl Accts  
* Industry Issues  
* News Room  
* Parts And Supplies  
* Systems  
* Training  
 
   

“Low-Flow” Coil Performance

Two objectives underlie the design of virtually every HVAC system: lower first cost and lower energy (life-cycle) cost. These goals are largely responsible for the growing popularity of “low-flow” chilled water systems. “Low-flow” designs provide required cooling capacity by using less water at colder temperatures, essentially trading an increase in chiller energy consumption for a greater reduction in pumping costs.

How does reduced water flow affect the performance of the cooling coil? An understanding of thermodynamics and the heat-transfer equation, Q = U × A × LMTD, tells us that less water flow through the coil tubes reduces heat-transfer coefficient U (waterside resistance to heat transfer increases). But as the graph illustrates, the log-mean temperature difference (LMTD) increases because the entering water temperature is colder.

The higher LMTD that accompanies low flow offsets the reduced heat-transfer coefficient. In effect, the capacity of the coil remains the same whether the water flow is 127 gal/min or 77 gal/min — without changing surface area A

Back to Log-Mean Temperature Difference or Table of Contents



© 2012 American Standard  All rights reserved