Commercial :  Local sales offices :  About Trane

 


* Book Store  
* Building Services  
* Case Studies  
* Engineers Newsletter  
* Products  
* Market Segments  
* Financing  
* Global/Ntnl Accts  
* Industry Issues  
* News Room  
* Parts And Supplies  
* Systems  
* Training  
 
   

Interconnecting Piping


Keep these general guidelines in mind as you review the recommendations specific to suction, liquid, discharge and hot gas bypass lines:

  • Limit overall line length, including the vertical suction and liquid risers. Enough subcooling may be lost as refrigerant travels up the liquid riser to cause flashing. Review any questionable applications with the manufacturer.

  • Use Type L copper tubing for R-22. For copper-to-copper joints, use BCuP-6 without flux. For copper-to-steel or copper-to-brass joints, use BAg-28 with a non-acid flux.

  • Rely on the equipment manufacturer to size the refrigerant lines. Only they know how the units interact with the system components.

  • If the manufacturer has not sized the refrigerant lines, use pipe sizing software such as Trane™ Engineering Toolbox to quickly determine proper sizes for refrigerant lines based on current engineering data.

Suction Line. Pressure drop in the suction line adversely affects unit capacity and efficiency. A pressure drop of 6 psid in matched commercial Trane RAUC units reduces system capacity by 2.5 percent and efficiency by 1.5 percent over the standard 3 psid design.

With that in mind, consider these suction-line recommendations:

  • Route the suction line from the evaporator to the compressor by the shortest path.

  • Use different pipe sizes for horizontal and vertical lines to make it easier to match line pressure drop and refrigerant velocity to suction-line requirements.

  • To assure proper oil entrainment and avoid sound transmission, size the suction line so that the refrigerant velocity equals or exceeds the required minimum velocity stated in Table 1 and remains below 4,000 fpm.

    Table 1
    Minimum Suction-Line Velocities
    for Oil Entrainment
    Refrigerant Velocity, fpm        
    Nominal
    Pipe Size, in.
    Riser Horizontal
    1-1/8 700 525
    1-3/8 780 585
    1-5/8 840 630
    2-1/8 980 735
    2-5/8 1080 810
    3-1/8 1180 885

  • Riser traps are unnecessary. If the riser is properly sized to maintain velocity, adding a trap only increases the suction- line pressure drop.

  • Double risers are unnecessary. The steps of unloading for commercial Trane units with scroll compressors are such that a single, carefully selected riser can maintain oil circulation at any load condition.

  • Even the most careful installation allows foreign matter into the system. That's why it's critical to install suction filters and properly maintain them. Once cleanup is complete, a fresh core should be installed in the shell to prevent oil trapping.

  • Figure 1 illustrates one method of trapping the evaporator coil. The suction lines from the evaporator headers should join at a point lower than the lowest suction header outlet. This arrangement drains the coils and prevents oil and refrigerant from “backfeeding” from one coil to the other(s).

    The common connection should then rise above the height of the coil before proceeding to the compressor to prevent the refrigerant and oil in the evaporator from “free-draining” toward the compressor. Figure 1: Recommended Suction-Line Arrangements from Evaporator Headers

  • Provide a 1-inch pitch toward the evaporator for every 10 feet of run to prevent any refrigerant that condenses in the suction line from flowing to the compressor when the unit is off.

  • Specify suction-line insulation if moisture condensation and dripping pose a problem, or to prevent refrigerant from condensing inside the lines if long runs will be exposed to low temperatures.

  • Don't install suction lines underground. The likelihood of corrosion, vibration, condensation of water outside—and refrigerant inside—the line, combined with inaccessibility and difficulty in maintaining cleanliness, make this practice unwise. If underground installation is unavoidable, make provisions to insulate, waterproof and encase the lines in a hard sleeve.

Liquid Line. Sufficient subcooling must be maintained at the expansion valve. To provide proper operation throughout the range of operating conditions, the liquid-line pressure drop should not exceed the unit's minimum subcooling value less 5°F. To achieve this objective, keep these liquid-line considerations in mind:

  • Select the smallest, practical line size for the application. Limiting the refrigerant charge improves compressor reliability.

  • When designing the liquid line for a typical air-conditioning application (i.e. one with an operating range of 40°F to 115°F), remember that every 10 feet of vertical rise will reduce subcooling by 2.8°F, while every 10 feet of vertical drop will add 1.1°F of subcooling.

  • Specify one expansion valve per distributor. An expansion valve serving more than one distributor will distribute the refrigerant unevenly.

  • Provide a 1-inch pitch toward the evaporator for every 10 feet of run. Since this pitch equals that of the suction line, the two may be run together.

    If the system is designed with a liquid line rise, a column of liquid refrigerant remains atop the volume of refrigerant gas in the condenser whenever the unit stops. The liquid refrigerant will eventually drain down the line and may fill the condenser ... perhaps even overflow to the compressor. Sloping the liquid line toward the evaporator creates a gas trap at the line's highest point, preventing liquid refrigerant from passing.

  • Solenoid valves are required. They prevent liquid refrigerant from filling the evaporator when the compressor stops and slugging when the compressor restarts. Adding solenoid valves also prevents siphoning which could allow an elevated column of liquid to overcome the gas trap and flow back into the condenser and compressor.

  • If the liquid line must be routed through an area warmer than outdoor air temperature, insulate the line to prevent the refrigerant from flashing.

  • Be sure to include a replaceable-core filter drier to permit proper system cleanup and moisture removal. The core should be changed whenever the system is opened for service.

  • Consider adding a moisture-indicating sight glass to permit a visual check of the liquid column for bubbles. However, never use the sight glass to determine whether It's prudent to avoid hot gas bypass in comfort cooling applications, especially those with variable-air-volume (VAV) systems.the system is properly charged! Instead, either charge the system based on the required subcooling or calculate the amount of refrigerant needed and add it based on weight.

Discharge Line. Limit the pressure drop in the discharge line to 6 psid whenever possible to minimize the adverse effect on unit capacity and efficiency. While a pressure drop of as much as 10 psid is usually permissible, note that a 6-psid pressure drop reduces unit capacity by 0.9 percent and efficiency by 3 percent.

To design the discharge line properly, follow the guidelines recommended below:

  • Choose the shortest route from the compressor to the condenser.

  • Use different pipe sizes for horizontal and vertical lines to make it easier to match line pressure drop and refrigerant velocity to discharge-line requirements.

  • To assure proper oil entrainment and avoid sound transmission, size the discharge line so that refrigerant velocity equals or exceeds the minimum velocity in Table 2 and remains below 3,500 fpm.

  • Prevent oil and condensed refrigerant from flowing back into the compressor during “off” cycles by: (a) pitching the discharge line toward the condenser and (b) routing the discharge line so that it rises to the top of the condenser, then drops to the level of the condenser inlet, creating an inverted trap.

  • Double risers are unnecessary. The scroll compressors in current Trane commercial units unload to the extent that a single, properly sized riser can transport oil at any load condition.

  • Riser traps are also unnecessary. Avoid using riser traps. If the discharge riser is sized to maintain the proper refrigerant velocity, adding a trap will only increase the pressure drop.

Hot Gas Bypass Line. “Hot gas bypass” (HGBP) describes the refrigerant system design historically used to provide stable operation at low loads while avoiding coil freeze-up and compressor cycling problems. When the load falls below the compressor's minimum stage of loading, the modulating HGBP valve attempts to maintain suction pressure by diverting hot gas from the compressor discharge to the evaporator inlet.

This strategy reduces the system's cooling capacity since the diverted refrigerant bypasses the evaporator. It also increases compressor energy consumption significantly and can cause unstable operation if improperly applied.

It's good design practice to avoid hot gas bypass for comfort cooling applications, particularly those with variable-air-volume (VAV) systems.

For other types of applications, observe these guidelines:

  • Size the HGBP line to carry only the desired amount of gas at a pressure drop equalling the sum (usually 20 to 40 psid) of the pressure drops for the discharge line plus the condenser and subcooler plus the liquid line. Oversizing the line can cause the HGBP and thermal expansion valves to “hunt.”

  • To assure proper oil entrainment, size the HGBP line so that refrigerant velocity equals or exceeds the minimum velocity recommended in Table 2.
Table 2
Minimum Discharge-Line Velocities
for Oil Entrainment
Refrigerant Velocity, fpm        
Nominal
Pipe Size, in.
Riser Horizontal
7/8 375 285
1-1/8 430 325
1-3/8 480 360
1-5/8 520 390
2-1/8 600 450

  • Elevate the HGBP valve above the discharge line and the distributor inlet to promote free drainage away from the HGBP valve and toward the distributor or discharge line.

  • Insulate the HGBP line to prevent the refrigerant from condensing during low loads.

Continue on to Bottom Line...

© 2012 American Standard  All rights reserved