Hospitality Success Stories

 

Successful Start of the Tourist Season

One week before Spring break, an exclusive hotel complex in Spain contacts Trane to repair their two broken-down chillers. With Holy Week coming up and very favorable weather with forecast temperatures above 25°C, their expectations of hotel occupancy were very high and needed a quick response.

The solution

  • 2 new CGAM 070 rental chillers
  • The Trane local Service team offered the hotel Maintenance Manager to rent two new CGAM-070 chillers while Trane proceeded with the repair of the damaged chillers. For the customer this was a very satisfactory suggestion. The quotes and order were processed in a few hours on Friday. The following Monday, the chillers were delivered on site and José Antonio Muñoz, Service Engineer from the Murcia Region quickly performed the installation and commissioning. On Tuesday both chillers were in service in the hotel.

    “The entire team worked together to give the best and fast solution to the customer,” said Angel Martínez, Service Sales Engineer of the Levante Region. “The customer is very satisfied with Trane level of service. They are now asking us to improve the hydraulic circuit of the site with a Trane Turnkey solution”.

 

Call to hire a rental unit now

 

+43 2236 378 400 00