Troubleshooting Your
Heating & Air Conditioning System before Service or Repair

It’s always nice when an expert is just a phone call away. There are, however, some quick and easy solutions you can try on your own. Below is a list of common issues, causes and remedies for HVAC systems. For anything that falls outside this list, see our Frequently Asked Questions section or contact your independent Trane dealer.

  • No cooling
    Potential cause First course of action Suggested solution
    You may have a tripped circuit breaker in your home Check your home circuit breaker box Reset circuit breaker
    Your thermostat may be off or set incorrectly Check to make sure your thermostat is on and set to cool Reset thermostat to your desired temperature
    Your indoor unit is running, but the outdoor unit is not Air coming through your vent will be warm. Check temperature setting Contact your local independent Trane dealer. In the meantime, try turning off your thermostat for 1–3 hours to see if it will reset
  • No heating
    Potential cause First course of action Suggested solution
    Your gas could be turned off Check gas valve at gas company meter, check shutoff valve at furnace, check for other shutoff valves Contact gas company to have gas valve turned on or contact your local independent Trane dealer
    Your system could be turned off or your unit unplugged Check your thermostat and system itself to assure that they are plugged in Refer to your use and care manual or contact your local independent Trane dealer
    Your thermostat may be off or set incorrectly Check to make sure your thermostat is on and set to heat Reset thermostat to your desired temperature
    You may have a tripped circuit breaker in your home Check your home circuit breaker box Reset circuit breaker box
  • No airflow
    Potential cause First course of action Suggested solution
    This may be the direct result of dirty filters Check the filters in each of your system components Clean or replace filters as recommended in your use and care manual. If problem persists, please contact your local independent Trane dealer
    Your system may have frozen up as the result of a dirty coil Check for signs of water below unit and cold exterior surface of indoor coil enclosure Contact your local independent Trane dealer. In the meantime, try turning your thermostat off for 1–3 hours to see if it will unfreeze
  • Unusually high utility bills
    Potential cause First course of action Suggested solution
    If your system is reaching its set point, is it working correctly?

    Are your local temperatures constantly in the extreme?
    Check the following:

    Is your system cycling constantly?

    Is your thermostat reaching its set value?

    Do you have any new appliances (e.g., a hot tub or pool heater) that are using lots of power?

    Have you checked to see if your local utility company had a recent rate increase?
    If your system is not reaching its set point, please contact your local independent Trane dealer
  • Equipment runs all the time
    Potential cause First course of action Suggested solution
    Your system could be trying to reach a set point that is too extreme. Check the set point on your thermostat. Is it very low (summer) or very high (winter)? Reset your thermostat. If that doesn’t work, please contact your local independent Trane dealer
  • Drain pan is overflowing
    Potential cause First course of action Suggested solution
    The overflow switch is probably not working Turn your system off Contact your local independent Trane dealer

SpringPromo2010

Save on your system this spring

36 Month No Interest* or 3.9% APR* or Up to $1,000 Rebate*